EcoStruxure IT forum
Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-02 11:05 AM . Last Modified: 2024-04-10 12:40 AM
I am trying to validate my network capacity calculations, in a simple data center with two racks, each of them have a patch panel in position 42 and a layer-2 switch in position 41:
From the capacity pie chart I can see that I have used 4% out of 24 ports available, approximately equal to 1 port. Thus I should have 23 ports available.
Now, if I look at the two racks in my data center, I would expect that I have only 22 ports available:
... since each switch has a used connection. In the left rack it is an "incoming" connection (from the server), in the right rack it is an "out-going" connection (to the layer 1 patch panel).
Each of the switches has 11 free ports that can be used for server equipment. Therefor I would expect the capacity pie chart to show a network utilization of approx. 8% (2 used ports out of 24 non-layer-1 ports).
In a larger data center this offset quickly scales to significant values.
Is the omission of connections to layer-1 equipment in the utilization calculation by intention?
--Christian
(CID:94602490)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-02 11:05 AM . Last Modified: 2024-04-10 12:40 AM
Hi Christian,
I looked into this, and it seems that for a port to count as used, it needs to be part of a complete route. A route does not terminate in a patch panel, so the starting port is not counted as used until the route is completed - i.e. something is plugged into the other side of the patch panel. I believe this is working as intended.
There does, however, seem to be a special case for routes between layer 2 and/or layer 3 network equipment - ports used in these routes are not counted as used. I will need to investigate further, whether there is a reason for this, or if this is unintended.
Regards,
Torben
(CID:94602632)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-02 11:05 AM . Last Modified: 2023-10-31 11:27 PM
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.