Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84854members
354323posts

NetBotz 570 MIB

EcoStruxure IT forum

A support forum for Data Center Operation, Data Center Expert, and EcoStruxure IT product users to share knowledge on installation, configuration, and general product use.

Solved
Mike-Sutton
Lieutenant JG
Lieutenant JG
0 Likes
5
675

NetBotz 570 MIB

Hi Does anyone have the MIB file for the NetBotz 570 and not the powernet MIB i mean the actual 570 version as I'm adding the system to a tonn interface and not having much joy at present.

 

TIA

 

Mike

Tags (1)

Accepted Solutions
APC_Steve
Commander Commander
Commander
0 Likes
1
659

Re: NetBotz 570 MIB

Hi @Mike-Sutton ,

 

If you go to the URL I provided, (changing <IP_of_NetBotz> to read the actual IP of the device) it will bring you to a text file. That file IS the MIB. You can simply right click that page and select save as. Save it as a text file and voila! you have the newest NetBotz MIB file. mib.PNG

 

This has nothing to do with the version of SNMP being used. SNMP version 1 and SNMP version 3 use the exact same MIB. NetbotzV3.mib is referencing the version 3 NetBotz appliances (355, 450, 455, 550, 570) and not the version of SNMP.

Regardless of the SNMP version used, you need the netbotzV3.mib as noted here:

http://www.apc.com/us/en/faqs/FA158368

 

Steve

See Answer In Context

Tags (1)
5 Replies 5
APC_Steve
Commander Commander
Commander
0 Likes
4
669

Re: NetBotz 570 MIB

Hi @Mike-Sutton ,

 

If you have the NetBotz 570, you actually already have the MIB:
http://<IP_of_NetBotz>/netbotzv3.mib

 

An appliance with the most recent firmware should also have the most recent MIB.

 

Thanks,

Steve

Tags (1)
Mike-Sutton
Lieutenant JG
Lieutenant JG
0 Likes
3
663

Re: NetBotz 570 MIB

Hi Steve,

 

TONN only talks v1 or v2 and Botz only talks v1 or v3 so it will be v1 tried running the script for the v1 mib but it didn't work that's why I'm asking for the file

 

Cheers,

 

Mike

Tags (1)
APC_Steve
Commander Commander
Commander
0 Likes
1
660

Re: NetBotz 570 MIB

Hi @Mike-Sutton ,

 

If you go to the URL I provided, (changing <IP_of_NetBotz> to read the actual IP of the device) it will bring you to a text file. That file IS the MIB. You can simply right click that page and select save as. Save it as a text file and voila! you have the newest NetBotz MIB file. mib.PNG

 

This has nothing to do with the version of SNMP being used. SNMP version 1 and SNMP version 3 use the exact same MIB. NetbotzV3.mib is referencing the version 3 NetBotz appliances (355, 450, 455, 550, 570) and not the version of SNMP.

Regardless of the SNMP version used, you need the netbotzV3.mib as noted here:

http://www.apc.com/us/en/faqs/FA158368

 

Steve

Tags (1)
APC_Steve
Commander Commander
Commander
0 Likes
0
658

Re: NetBotz 570 MIB

.S.
I checked the SE.com site and found this:

https://www.se.com/us/en/product/SFNBMIB410/netbotz-mib-v4.1.0/

 

Same file, likely same version.

Tags (1)
Shaun
Lt. Commander Lt. Commander
Lt. Commander
0 Likes
0
653

Re: NetBotz 570 MIB

Hi Mike,

 

If your application refuses to believe this is snmp-v1, it may work if you set it as snmp-v2c.  There's a weird (and rare) edge-case of apps that don't like using snmpv2 primitives in snmpv1.  v2c should be compatible enough to circumvent this.

 

(You can see this in Steve's screenshot, the first few lines end with "from SNMPv2-TC" and SNMPv2-SMI. Some very, very fussy applications don't like that.)

Tags (1)