Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84606members
353882posts

Invalid Network Address or time out on DCE Client

EcoStruxure IT forum

A support forum for Data Center Operation, Data Center Expert, and EcoStruxure IT product users to share knowledge on installation, configuration, and general product use.

Solved
AhmedAzzam2200
Crewman Crewman
Crewman
0 Likes
5
1152

Invalid Network Address or time out on DCE Client


Hi Everyone,

 

I have an issue in DCE Client V7.8.1 when I try to Log in DCE server by DCE Client, I get the error ( Invalid Network Address or time out) in DCE Client. while I Can access the server by the web as shown in the attached Pics.

I tried to increase the time out, change the port number, using HTTP and HTTPS ports and they didn't work yet.

 

Thanks in advance,

Attachments
Tags (1)

Accepted Solutions
Jef
Captain Captain
Captain
2
1041

Re: Invalid Network Address or time out on DCE Client

Hi Ahmed,

 

Try checking the client logs to see if there should be any useful info. Client log file usually located in Win. C:\Users\<username>\.isxc\7.8.1\.metadata\.log

 

If the client is unable to connect to server, then it might be network/routing related. Maybe something like firewall, antivirus program, proxy server, VPN, etc. 'located' between the client and server not permitting the desktop client to connect (but permitting the http/https connections).

 

Kind regards,

Jef

See Answer In Context

Tags (1)
5 Replies 5
Jef
Captain Captain
Captain
0 Likes
4
1114

Re: Invalid Network Address or time out on DCE Client

Hi Ahmed,

 

It seems you are trying to connect (login) to servers private LAN, that is not supported for desktop client access.

Assuming the server is configured/setup properly, it should usually have 2 network interfaces: Public (LAN1) and Private (LAN2). 
You can try to login via the IP address for the Public/LAN2 that you have assigned (configured during the installation).

 

Kind regards,

Jef

Tags (1)
AhmedAzzam2200
Crewman Crewman
Crewman
0 Likes
3
1059

Re: Invalid Network Address or time out on DCE Client

Dear Jef,

 

I tried to connect to the server through Private and public Networks and it doesn't work for both.


Thanks.

Tags (1)
Jef
Captain Captain
Captain
2
1042

Re: Invalid Network Address or time out on DCE Client

Hi Ahmed,

 

Try checking the client logs to see if there should be any useful info. Client log file usually located in Win. C:\Users\<username>\.isxc\7.8.1\.metadata\.log

 

If the client is unable to connect to server, then it might be network/routing related. Maybe something like firewall, antivirus program, proxy server, VPN, etc. 'located' between the client and server not permitting the desktop client to connect (but permitting the http/https connections).

 

Kind regards,

Jef

Tags (1)
AhmedAzzam2200
Crewman Crewman
Crewman
0 Likes
1
998

Re: Invalid Network Address or time out on DCE Client

Dear Jef,

thank You for Your replay actually, I checked it and  it was a problem with Antivirus Firewall as you said, Thanks a lot

Thanks

Tags (1)
Jef
Captain Captain
Captain

Re: Invalid Network Address or time out on DCE Client

Hi Ahmed,

 

You are welcome & many thanks for the update.

 

Kind regards,

Jef

Tags (1)