Ask Me About Webinar: Data Center Assets - Modeling, Cooling, and CFD Simulation
Join our 30-minute expert session on July 10, 2025 (9:00 AM & 5:00 PM CET), to explore Digital Twins, cooling simulations, and IT infrastructure modeling. Learn how to boost resiliency and plan power capacity effectively. Register now to secure your spot!
EcoStruxure IT forum
Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-02 09:02 AM . Last Modified: 2024-04-10 01:20 AM
Hello,
I would like to buy some Netbotz PS100 dust sensors but it is not really clear how to connect those to get the data.
On the documentation I found, it is said that I should use a sensor pod 120 to connect this sensor, but this sensor pod is not sold anymore.
The thing is that I need a test setup for 1 or 2 PS100 sensors and need to get the minimal required infrastructure to read the measurements.
I could not get any documentation about this sensor (sensibility, number of channels, size of the measured particles...), so it is difficult to justify the investment in a full Netbotz infrastructure without this documentation.
Basically what do I need to buy minimally? Would a PS100 alone be enough? A PS100 + sensor pod 155? A PS100 + rack monitor XXX? a PS100 + netpod XXX + rack monitor XXX?
Thank you for your answers.
(CID:92078121)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-02 09:02 AM . Last Modified: 2024-04-10 01:20 AM
Hello Julien,
Thanks for your post. To get this working you would need to invest in a Netbotz appliance from the 4xx or 5xx ranges and also purchase a NBPD0122 (although it does show on the website that this is discontinued, it is available for the foreseeable future, from a Reseller or by contacting the sales department in your local region). This is the only way this PS100 sensor will work with the V3 Netbotz appliances.
information on the PS100 is below:
http://www.apcmedia.com/salestools/ASTE-6Z5S83/ASTE-6Z5S83_R0_EN.pdf
Also we do have another option for you. We can integrate 3rd party sensors to these appliances using the 0-5v and 4-20mA sensor options. If there is another particle sensor you wish to connect to the Netbotz appliance you can do this using the other sensor options.
Regards,
Breda
(CID:92078130)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-02 09:02 AM . Last Modified: 2024-04-10 01:20 AM
Hi Julien
We have both items if you need them, I will check on Monday but I think the NBPD0122 will also work with the NeyBotz 450, 455 and 570.
Regards
Aaron
aaron@ ecl-ips.com
ecl-ips.com
(CID:92536921)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-02 09:02 AM . Last Modified: 2024-04-10 01:20 AM
Julien,
I just installed two of the PS100 sensors. The PS100 connects to an older sensor pod 120, which we purchased off an auction site. The sensor pod 120 then connects to our NB570. I am also using a USB to cat5 extender to connect the sensor pod 120 to the NB570 which is around 100 feet away.
It all works very well.
David
(CID:93914560)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-02 09:02 AM . Last Modified: 2023-10-31 11:00 PM
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Welcome to your new personalized space.
of