Posted: 2020-07-05 03:50 PM . Last Modified: 2024-04-03 11:17 PM
Does the AP7911B PDU not have the ability to track Total Power kVA like the AP8941?
Someone suggested that I needed to update the DCE to 7.6, which would give me the most current DDFs. I have updated the DCE to 7.6 and also updated the PDU firmware and I still don't see the kVA sensor.
(CID:137729412)
- Labels:
-
Data Center Expert
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
Posted: 2020-07-05 03:50 PM . Last Modified: 2024-04-03 11:17 PM
Hi Krista,
I checked an AP7911B via SNMP using the following OID:
hardware.rPDU2.rPDU2Phase.rPDU2PhaseStatusTable.rPDU2PhaseStatusEntry.rPDU2PhaseStatusVoltage
The return was a -1. This indicates that voltage is not supported by this device. Without voltage, you can not get wattage. The DDF can not calculate it outside of the device as it will do in some instances. The device does support current, but not wattage or voltage.
rPDU2PhaseStatusPower also reports a -1
It simply appears that this device does not support a watt or KW sensor.
Thanks,
Steve
(CID:137729428)
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
Posted: 2020-07-05 03:50 PM . Last Modified: 2024-04-03 11:17 PM
Dear Krista Flynn,
Tell us, please, did you solve your question or not?
With respect.
(CID:139693981)
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
Posted: 2020-07-05 03:50 PM . Last Modified: 2023-10-22 01:56 AM
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Link copied. Please paste this link to share this article on your social media post.