EcoStruxure IT forum
Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-03 08:35 AM . Last Modified: 2024-04-08 03:49 AM
I am trying to upgrade DCO from v8 to v8.0.1 and it fails with the following error shown below.
I have tried ticking both the "Do not download packages from the Internet" and "No thirdparty RPMs" but it still doesn't succeed.
done
Install GPG key...
done
Cleaning yum cache
Loaded plugins: fastestmirror
Cleaning repos: base centos-specific-swdco-local-rpms extras swdco-local-rpms
: thirdparty-swdco-local-rpms updates
Cleaning up everything
Updating packages
Loaded plugins: fastestmirror
One of the configured repositories failed (Unknown),
and yum doesn't have enough cached data to continue. At this point the only
safe thing yum can do is fail. There are a few ways to work "fix" this:
1. Contact the upstream for the repository and get them to fix the problem.
2. Reconfigure the baseurl/etc. for the repository, to point to a working
upstream. This is most often useful if you are using a newer
distribution release than is supported by the repository (and the
packages for the previous distribution release still work).
3. Disable the repository, so yum won't use it by default. Yum will then
just ignore the repository until you permanently enable it again or use
--enablerepo for temporary usage:
yum-config-manager --disable
4. Configure the failing repository to be skipped, if it is unavailable.
Note that yum will try to contact the repo. when it runs most commands,
so will have to try and fail each time (and thus. yum will be be much
slower). If it is a very temporary problem though, this is often a nice
compromise:
yum-config-manager --save --setopt=.skip_if_unavailable=true
Cannot find a valid baseurl for repo: base/7/x86_64
Could not retrieve mirrorlist http://mirrorlist.centos.org/?release=7&arch=x86_64&repo=os&infra=stock error was
14: curl#7 - "Failed to connect to 2001:4178:5:200::10: Network is unreachable"
removing update repositories
Removing DCO yum repository...
done
Removing third party centos specific yum repository...
done
Removing third party yum repository...
done
done
Operations::UpgradeManager::validateUpgrade Validating upgrade...
Operations::UpgradeManager::cleanupAndExit Upgrade failed with: Build info did not match installer. Expected: 5874f3e3e97282375f22f6f54aa460d76e77b477 Got: 1c8935eaf80f40eb7d9b78170dffbd18fdf9b266
Operations::UpgradeManager::umountIso Unmount ISO
Operations::OperationsLib::removeFile Removing file '/var/run/dco/upgrade-running'
Operations::UpgradeManager::restart The upgrade process is now complete.
Platform.pm completed run-upgrade in 53.4574720859528 secs with exit value: 0.
(CID:110006584)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-03 08:35 AM . Last Modified: 2024-04-08 03:49 AM
Hi Chad,
Perhaps the installation files(s) are damaged/corrupted, logs complaining about the installer/build info not matching ... however I would suggest if possible using the latest release, currently DCO 8.0.2 for the product upgrade. I would also suggest to upload the installation file(s) to server local disc, eg. run the installer from the local disk (and not from a network drive). You might also want to try the upgrade by only selecting/ticking the option "Do not download packages from the Internet" (and leave the 'No thirdparty RPMs" un-ticked).
Kind regards
(CID:110006807)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-03 08:35 AM . Last Modified: 2024-04-08 03:49 AM
In my case the non obligatory check box - Do not download packages from the Internet
must be checked! 😀
I made the upgrade from v.8.0.1 to v.8.0.3.
(CID:110017472)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-03 08:35 AM . Last Modified: 2023-10-22 01:46 AM
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.