Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84494members
353715posts

DCO rack elevation items

EcoStruxure IT forum

A support forum for Data Center Operation, Data Center Expert, and EcoStruxure IT product users to share knowledge on installation, configuration, and general product use.

Carmine
Cadet
0 Likes
3
717

DCO rack elevation items

I would like to see if a report could be added to DCO that shows the rack elevations along with the item that is in that U space. Currently DCO has a report that shows  rack u space front and rear and what is used and free but does not depict the item in the used u space. 

 

It would be nice if It show the physical device being used in that space. 

 

Thanks,

Carmine

Tags (1)
3 Replies 3
gsterling
Commander Commander
Commander

Re: DCO rack elevation items

Hello Carmine

 

We can add your feedback to other feedback for the reporting team if you'd like.

 

DCO/ITA is also capable of outputting the rack views to a file if that would work for you on the short term. To do so you'll notice in the room view there's an "export layout as image" button above the pad lock button when in planning mode or the pointer button when in operations mode

 

When you select that option you can choose "rack view". You'll then have the option to output based on the racks you've selected or a row-level view of the selected racks. So you can do an entire room in one selection to get output like this below.

 

RackView-1.JPG

 

As mentioned, we will forward your feedback to the prod management team for consideration in future reporting.

 

Regards

 

Greg Sterling

Tags (1)
Ariane
Cadet
0 Likes
0
687

Re: DCO rack elevation items

Thanks for the update and quick reply. I'll be sure to keep an eye on this thread MyFordBenefits Login

Tags (2)
Carmine
Cadet
0 Likes
0
681

Re: DCO rack elevation items

Thanks Greg for the information. I will try just that on my end. Will see if management is ok with this method.

 

Regards,

Carmine

 

Tags (1)