Ask our Experts
Didn't find what you are looking for? Ask our experts!
Share Your Feedback – Help Us Improve Search on Community! Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately. Click here to take the survey
Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
Search in
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-04 03:35 PM . Last Modified: 2024-04-05 12:31 AM
Good afternoon all,
we continue to be experiencing an issue where our Virtual DCE 7.3.1 generates a multitude of communication lost alarms across multiple device types.
It seems that the lost connectivity alarms are mostly generated during the late evening or overnight hours, with hardly any occurring during business hours.
I was told it is possibly a latency issue given the server is located in one city and the the devices are spread out as far as other cities 350 Kilometers away that could be causing these timeouts.
I checked the KBase, to see if anyone had added similar topic, recently and noticed: . My issue is essentially the same except on version 7.3.1... using SNMPv1 and although some devices have up to date firmware the lost connectivity still occurs on them also.
Any assistance, guidance or suggestions with this issue would be greatly appreciated in the meantime I will a closer look at the above example and see if I have missed any of the steps that were offered above.
Thank you in advance,
Mark
(CID:129409954)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-04 03:35 PM . Last Modified: 2024-04-05 12:31 AM
Hi Mark,
Intermittent SNMP issues can be difficult to pin down but if it's happening at certain times a day, that may make it easier. First, take a look at the following k-base:
http://www.apc.com/us/en/faqs/FA226273/
That goes through some basics of troubleshooting SNMP. If you think it is a latency issue, things like timeouts and retries should potentially be increased as noted in the document.
You may also want to take a look a the logs on the devices themselves. Are there other systems polling the devices at that time? Perhaps another NMS trying numerous community names if SNMP V1? The newest firmware on APC devices should be able to indicate if there is such an issue by showing unauthorized attempts.
You may also want to look at other network activities at this time. Is there a great deal more traffic due to backups and vulnerability sweeps?
You may also want to consider getting DCE up to date. We're up to 7.5 now and there have been updates to things like SNMP processes. The issues noted in the post you mentioned would not likely be the same as SNMP version 1 and version 3 issues are different and that was version 3 specific. Still, it's best to be up to date on all aspects.
If these issues are happening at a certain time, you can also look at things on the DCE server that may be set to happen overnight such as backups being performed, discoveries set to run, etc. If the issues are happening to specific locations however, it's more likely that it is network based than server based.
Steve
(CID:129412223)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-04 03:35 PM . Last Modified: 2024-04-05 12:31 AM
Hi Mark , thanks for posting. Let's hope you find your answer here.
Kind regards Ditte
(CID:129412062)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-04 03:35 PM . Last Modified: 2024-04-05 12:31 AM
Hi Mark,
Intermittent SNMP issues can be difficult to pin down but if it's happening at certain times a day, that may make it easier. First, take a look at the following k-base:
http://www.apc.com/us/en/faqs/FA226273/
That goes through some basics of troubleshooting SNMP. If you think it is a latency issue, things like timeouts and retries should potentially be increased as noted in the document.
You may also want to take a look a the logs on the devices themselves. Are there other systems polling the devices at that time? Perhaps another NMS trying numerous community names if SNMP V1? The newest firmware on APC devices should be able to indicate if there is such an issue by showing unauthorized attempts.
You may also want to look at other network activities at this time. Is there a great deal more traffic due to backups and vulnerability sweeps?
You may also want to consider getting DCE up to date. We're up to 7.5 now and there have been updates to things like SNMP processes. The issues noted in the post you mentioned would not likely be the same as SNMP version 1 and version 3 issues are different and that was version 3 specific. Still, it's best to be up to date on all aspects.
If these issues are happening at a certain time, you can also look at things on the DCE server that may be set to happen overnight such as backups being performed, discoveries set to run, etc. If the issues are happening to specific locations however, it's more likely that it is network based than server based.
Steve
(CID:129412223)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-04 03:35 PM . Last Modified: 2023-10-22 01:10 AM
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.