Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Device Configuration and Firmware Update

EcoStruxure IT Forum

Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
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
  • Device Configuration and Firmware Update
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Cory_McDonald
Cory_McDonald Champion
159
Jef
Jef Leader
114
gsterling
gsterling Mentor
77
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
Back to EcoStruxure IT Forum
Start a Topic
apachecav
apachecav
Explorer

Posted: ‎2023-12-21 11:05 AM

0 Likes
1
992
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
Posted: ‎2023-12-21 11:05 AM

Device Configuration and Firmware Update

Does each UPS need their own credentials for setting the SCP/FTP in the 

Device Configuration and Firmware Update in the gateway like in the polling section or will one global one do?

Labels
  • Labels:
  • IT Expert
  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic
Reply 1
Cory_McDonald
Cory_McDonald Champion
Champion

Posted: ‎2024-05-02 04:57 AM

0 Likes
0
832
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
Posted: ‎2024-05-02 04:57 AM

Hi @apachecav,

 

The credentials for FTP/SCP that are stored in the Device Configuration and Firmware Updates section of the Gateway are credentials that could potentially be used to connect to any device via FTP/SCP that is discovered by the gateway. 

 

If you add a new set of credentials or modify an existing set of credentials you will need to rerun a discovery (no need to delete the device) and the new set of credentials will be used.  This means that when the discoveries are ran, the Gateway will determine which set of credentials works for a device.

 

Just a note that if you end up with a lot of credentials in your list, it is recommended to change the discovery settings for Configure credentials to only have the specific set of credentials selected that apply to the device.

 

Additional information on managing the credentials as well as when a discovery needs to be re-ran can be found here: https://community.se.com/t5/Configuration/Configure-Gateway-device-file-transfer-settings/ta-p/44689...

 

Thanks,

Cory
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.