Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84454members
353658posts

Suggestion: Video Integration

EcoStruxure Geo SCADA Expert Forum

Find out how SCADA systems and networks, like EcoStruxure Geo SCADA Expert, help industrial organizations maintaining efficiency, processing data for smarter decision making with IoT, RTU and PLC devices.

Solved
MikeForshock
Lieutenant JG
Lieutenant JG
0 Likes
10
2767

Suggestion: Video Integration

In some previous (legacy) platforms we had the ability to embedded video (RTSP, HTML) typically though the old OLE/ActiveX platform.

We have used the Remote Image option to update snapshots on a specific interval or action, but a live video option would certainly be a great addition for some applications. With the new HTML5 Virtual Client now part of 2019, maybe progress will be made to implement a HTML5 Video element that can use the codecs available on the machine.

 

Just a simple request or suggestion, for now we launch a dedicated VMS viewer.


Accepted Solutions
MikeForshock
Lieutenant JG
Lieutenant JG
0 Likes
2
440

Re: Suggestion: Video Integration

Chrome/WebKit is now used for the internal web page viewer as of version 2021.

 

Cannot do a download function, but most other functions appear to work (new window, responsive layouts).

 

 

See Answer In Context

10 Replies 10
JChamberlain
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
3
2759

Re: Suggestion: Video Integration

You can open hyperlinks to web pages in ViewX, so if the video is on a page already it should work.

MikeForshock
Lieutenant JG
Lieutenant JG
0 Likes
0
2688

Re: Suggestion: Video Integration

Correct, you can force the default browser to open. We do this often to load external reporting and video connections

I am hoping more along the lines of embedding actual video in the mimic.

richardonline
Cadet
0 Likes
1
2509

Re: Suggestion: Video Integration

@JChamberlain thanks for sharing your thoughts .its working 

Tags (1)
BevanWeiss
Spock
Spock
0
2475

Re: Suggestion: Video Integration

Having an embedded video player within ViewX would still be good though 😉


Lead Control Systems Engineer for Alliance Automation (VIC).
All opinions are my own and do not represent the opinions or policies of my employer, or of my cat..
Tags (1)
MikeForshock
Lieutenant JG
Lieutenant JG
0 Likes
2
2453

Re: Suggestion: Video Integration

Since it appears Chromium/WebKit (Chrome, Edge (New), Operara, etc.) will now rule the world why not join the party with the integrated viewer:

 

Chromium Embedded Framework.

https://bitbucket.org/chromiumembedded/

 

Has links to using with .Net, Delphi, Java and others.

 

Allows embedding the web browser similar to how the ViewX currently embeds the IE ActiveX control.
A little bit of work and can keep security going.

Nearly every VMS and other machine vision camera works well inside a browser.

 

Allow a Inset window with the ViewX instead of only allowing a new or navigate and this will be easy to begin integration.

 

Tags (1)
BevanWeiss
Spock
Spock
1
2446

Re: Suggestion: Video Integration

Hi @MikeForshock 

I'm not sure that ViewX has ActiveX anymore.  I know that it did have it (albeit unsupported) back in 2013 era (and prior), but I'm pretty sure when they migrated up to the 2014/2015 platform and had the major UI revamp it was dropped completely.

 

ViewX does actually already have a Chromium component, it's used to popout the GeoSpatial maps.  But these also aren't capable of being embedded into a ViewX Mimic at this stage (although I've got a few feature requests that I've submitted around this).

 

Definitely worth sending in feature request tickets in my opinion (to your local Tech Support contact).  Without feedback from End Users / System Integrators on what direction the product 'should' take, it becomes a guessing game for Schneider/AVEVA.

 


Lead Control Systems Engineer for Alliance Automation (VIC).
All opinions are my own and do not represent the opinions or policies of my employer, or of my cat..
Tags (1)
MikeForshock
Lieutenant JG
Lieutenant JG
0 Likes
0
2444

Re: Suggestion: Video Integration

Interesting they would have Chromium support for the Geo/Maps but use the old OLE/ActiveX web component for displaying hyperlinks in ViewX:

HTTP USER AGENT: Mozilla/4.0 (compatible; MSIE 7.0; Windows NT 6.2; WOW64; Trident/7.0; .NET4.0C; .NET4.0E; .NET CLR 2.0.50727; .NET CLR 3.0.30729; .NET CLR 3.5.30729; Tablet PC 2.0)

 

I am aware they no longer allow ActiveX integration within the ViewX and dont want that back haha.

 

 

Tags (1)
MikeForshock
Lieutenant JG
Lieutenant JG
0 Likes
2
441

Re: Suggestion: Video Integration

Chrome/WebKit is now used for the internal web page viewer as of version 2021.

 

Cannot do a download function, but most other functions appear to work (new window, responsive layouts).

 

 

BevanWeiss
Spock
Spock
0 Likes
1
431

Re: Suggestion: Video Integration

It can't be nested within a normal Mimic display though right? (I've got 2021 installed, but haven't used it much).

If it supported a nested HTML 'viewer' (i.e. a display element on a standard Mimic that could be set with a URL) that would be great...


Lead Control Systems Engineer for Alliance Automation (VIC).
All opinions are my own and do not represent the opinions or policies of my employer, or of my cat..
sbeadle
Janeway Janeway
Janeway
0 Likes
0
427

Re: Suggestion: Video Integration

No Bevan, though that has been lodged as an enhancement request.