Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
It's your place to connect with experts and peers, get continuous support, and share knowledge.
Find out how SCADA systems and networks, like EcoStruxure Geo SCADA Expert, help industrial organizations maintaining efficiency, processing data for smarter decision making with IoT, RTU and PLC devices.
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2020-10-14 08:23 AM
Im testing the XML SOAP with a simple SQL Query, however Im not sure if Im using the correct syntax because i cant see the data and the software prompt some errors.
The software used is SOAPUI 5.6
<soapenv:Envelope xmlns:soapenv="http://schemas.xmlsoap.org/soap/envelope/" xmlns:scx6="http://serck-controls.com/webservices/SCX6/">
<soapenv:Header/>
<soapenv:Body>
<scx6:ExecuteQuery>
<scx6:SQL>SELECT TOP(5) FULLNAME FROM CDBPOINT</scx6:SQL>
</scx6:ExecuteQuery>
</soapenv:Body>
</soapenv:Envelope>
The connection configured is http://localhost:85/webservices/scx
Posted: 2020-10-14 09:04 PM
I think your endpoint URL is wrong.
http://localhost:85/webservices/scx
I think this should most likely just be:
http://localhost/webservices/scx
IIF you allow insecure HTTP... otherwise you could go with https://localhost/webservices/scx
The reason I think 85 is wrong is that if you installed the 'new' (old) IIS-based WebX then it will also install itself at port 85, and this will conflict with your ClearSCADA WebX which defaults to port 80, but which you say you have configured as port 85.
Posted: 2020-10-15 09:39 PM
Hello bevan
I changed the port for webX to 80 and checked the option for insecure http from the server configuration, but the software still prompt errors.
Could be the syntax?
Posted: 2020-10-16 10:26 PM
I'd recommend that you start with something a bit more structured before you go hand creating the SOAP requests
I believe that you could even directly import in the Web Service references if you're using a recent version of Visual Studio, and your Visual Studio environment has access to the ClearSCADA (or Geo SCADA Expert) server.
Then once you have something working, you could use wireshark or similar to snoop on the traffic to get the structure of the requests / responses.
I think you should also go back to first principles with your fault finding. You say 'the software still prompts errors'... that means literally nothing. Does this error say 'Buy a licence to use this software'??.. because if so, maybe you solve the problem by buying a licence to use the software... (SOAP UI is free-to-use software.. so I suspect it's not this, but you also clearly haven't told us either way..)
So start from the beginning, things like
Posted: 2020-10-30 07:58 AM
Answer to your questions
So start from the beginning, things like
I tried with the code below. I can execute the query when the database is accesible by the guest user, when i configure the security, even using the object System.Net.NetworkCredential, the query is null.
object[] obj;
SOAPconsole.localhost.SCXService MySoap;
MySoap = new SOAPconsole.localhost.SCXService();
MySoap.Url = "http://localhost/webservices/scx";
System.Net.NetworkCredential userDefined = new System.Net.NetworkCredential("User","Password");
MySoap.Credentials = userDefined;
try {
obj = new object[0];
bool limit;
bool size;
object[][] retobj;
retobj = MySoap.ExecuteQuery("Select fullname from CDBObject", obj, out limit, out size);
Console.WriteLine("Query executed. Number of elements polled: " + retobj.Length);
for (int i = 0; i < retobj.Length; i++)
Console.WriteLine(retobj[i][0].ToString());
}
catch (Exception ex) {
Console.WriteLine(ex.Message);
}
Console.ReadLine();
Posted: 2020-11-01 05:37 PM
What does Wireshark say when you look at the traffic?
I suspect that your authentication isn't working.
I doubt that ClearSCADA will return a 401 'Authorization Request', since technically for that URL the Guest user (i.e. no authentication user) does have certain authorization, just typically it will be so low that it's meaningless (i.e. no visibility/browse permissions for any objects).
You probably just want to force the authentication elements into the request header rather than trying to use the NetworkCredentials.
Posted: 2021-04-07 10:47 PM
I've learnt new things about the SOAP interface.
Even though SOAP itself has an authentication method available (WS-S), Geo SCADA Expert instead uses cookies.
What is required is to send a PUT to /logon with a body of
username={USERNAME}&password={PASSWORD}&redir=/
This will then provide you some cookies which should be sent alongside every other HTTP request.
This info came from the Node-RED stuff that Steve Beadle did here:
https://github.com/GeoSCADA/Node-Red-GeoSCADA/blob/master/GeoSCADA.js
It looks like the cookies have an expiry time also, so it may require some additional consideration around that.
User | Count |
---|---|
199 | |
80 | |
36 | |
23 | |
18 | |
12 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.