New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
[Imported] Using Bulk edit tool for Editing Instances
EcoStruxure Geo SCADA Expert Forum
Schneider Electric support forum about installation, configuration, integration and troubleshooting of EcoStruxure Geo SCADA Expert (ClearSCADA, ViewX, WebX).
Search in
Improve your search experience:
Exact phrase→Use quotes " "(e.g., "error 404")
Wildcard→Use * for partial words(e.g., build*, *tion)
AND / OR→Combine keywords(e.g., login AND error, login OR sign‑in)
Keep it short→Use 2–3 relevant words, not full sentences
Filters→Narrow results by section(Knowledge Base, Users, Products)
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
You have entered an invalid email address. Please re-enter the email address.
This co-worker has already been invited to the Exchange portal. Please invite another co-worker.
Please enter email address
Send InviteCancel
Invitation Sent
Your invitation was sent.Thanks for sharing Exchange with your co-worker.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2019-10-2602:16 AM. Last Modified: 2023-05-0312:39 AM
[Imported] Using Bulk edit tool for Editing Instances
>>Message imported from previous forum - Category:Bulk Edit Tool<< User: mchartrand, originally posted: 2018-10-19 13:22:38 Id:142 This is a re-posting from the obsoleted (October 2018) "Schneider Electric Telemetry & SCADA" forum. The original posters' identities have not been included. Schneider Electric is not responsible for the content of these posts.
-------------------------------
**_I am using Clear scada 2015 r2. I used Bulk edit tool to make changes to the Template which was successful. But can we make changes to Object Instances as well. I cannot see any object instance in the tool though. Please help._**
__________________________________
The BulkEdit user Guide is in the start menu, you might find helpful. There are two basic editing functions BulkEdit does. Edit Poperty settings in any object in the database, and edit Property Overrides in the template(s).
There is a bug in Bulk Edit at startup. It starts up with the template database tree that is for editing property overrides but loads the code to edit the object properties. So to get it to behave right, when you first start it, you have to select which form of editing you want to do.
On the button toolbar the first button has the ClearSCADA database Icon, and is for Logout and Reload Database, the second button loads the Properties editing, and the third button loads the Property override editing.
Use the second button to load the properties editing to edit the instances properties.
__________________
**_That was helpfull. Thank you for the response._**
___________________
You are welcome. That bug had me going nuts until I figured it out, sometimes it worked as I expected and others it did not.