Ask our Experts
Didn't find what you are looking for? Ask our experts!
Share Your Feedback – Help Us Improve Search on Community! Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately. Click here to take the survey
Schneider Electric support forum about installation, configuration, integration and troubleshooting of EcoStruxure Geo SCADA Expert (ClearSCADA, ViewX, WebX).
Search in
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-12-09 01:47 PM
Hi everyone! I'm trying to read variables using Geo SCADA as a client to an OPC DA server, but I can't even establish a connection. I've tried all the available OPCs in Geo SCADA—OPC Simple, OPC Advanced, OPC XLM-DA, but none of them detect the server. Does anyone have any suggestions?
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-12-09 02:41 PM
Is the OPC server on the same machine as Geo SCADA or remote?
If remote, are you using a tunnel or directly connecting to the remote IP?
If local, can third party OPC clients connect?
What errors do you get?
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-12-09 09:22 PM . Last Modified: 2025-12-09 09:24 PM
There's no point trying to use OPC XML-DA if your server is only OPC-DA. OPC XML-DA is an entirely different 'protocol' than OPC-DA...
Your issue is almost certainly going to be DCOM security related. Especially if you're using an up to date operating system on the OPC-DA Server end.
If you can change your OPC-DA server over for OPC-UA things will be so very much easier.
Likewise if you can change your OPC-DA server over for OPC XML-DA.. both of these avoid DCOM, and you do really want to avoid DCOM.
If you're really stuck with OPC-DA, then you're going to want to start looking up on DCOM, and DCOM security.
To browse for the remote OPC-DA server, you will need to allow for remote start and access to OpcEnum on the remote machine. If both OPC-DA server and client are on the same domain, then you can use domain authentication, and configure the DCOM authorization based on this. If they're not... then things start to get much sketchier... sometimes it works if you create a local user on the OPC-DA server, give that permissions for OpcEnum and the server that you need to expose, and then make sure that the OPC-DA client passes through a username/password for authentication.
Often I just end up opening up OpcEnum to anonymous users.. which is terrible from a security perspective.
Really really really try to get OPC-UA instead. It's really so much easier.
Ohh.. or you can try either KepWare / Matrikon OPC Tunnellers
https://www.opcturkey.com/uploads/kepserverex-opc-tunnel.pdf
https://www.matrikonopc.com/opc-ua/products/opc-ua-tunneller.aspx
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-12-10 08:04 AM
Hi Adam, about your questions:
1. the server is remote
2. I'm connecting directly by IP addressing
3. I tested a local connection using a third party opc client and it worked good.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-12-10 08:09 AM
Hi Bevan, thank you for your answer, but unfortunately I'm stuck with OPC DA server. I'll check the information in the links you sent me.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-12-10 04:53 PM . Last Modified: 2025-12-10 04:55 PM
Then what Bevan says about DCOM is likely your hurdle and has been since WinXP SP2... follow his suggestions and see what you can get sorted
Side note, if the remote server is also ClearSCADA/Geo SCADA, configuring ViewX also sets up a tunnel bypassing the headache of DCOM. If you configure ViewX at the client machine to connect to the remote server (hide it from ViewX if you want) and then point your OPC client to 127.0.0.1
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.