Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Device configuration - Gateway versions 1.24 and older

Device configuration
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
  • EcoStruxure IT Help Center
  • EcoStruxure IT Help Center Categories
  • IT Expert
  • Configuration
  • Device configuration
  • Device configuration - Gateway versions 1.24 and older
Options
  • Mark as New
  • Mark as Read
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
  • Video: Device configuration
  • Device configuration - Gateway versions 1.24 and o...
  • NMC user configuration in IT Expert
  • Video: Device configuration
  • Device configuration - Gateway versions 1.24 and o...
  • NMC user configuration in IT Expert

Related Forums

  • EcoStruxure IT Forum

  • APC UPS Data Center & Enterprise Solutions Forum

Previous Next

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite

EcoStruxure IT Support

Submit a support request for additional assistance with EcoStruxure IT software.

Request Support
Back to Device configuration
Start a Topic
Options
  • Mark as New
  • Mark as Read
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
1 Like
410 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Device configuration - Gateway versions 1.24 and older

Sisko JLehr Sisko
‎2025-06-16 09:34 AM

 

If all the Gateways in your organization run software version 1.24 and older, Device configuration is available without the newest features.

 

To access the newest Device configuration features in IT Expert, all EcoStruxure IT Gateways in your organization must be updated to version 2.0 or newer.

 

Auto-update to Gateway version 2.0.1 is being rolled out in stages. Manual update to version 2.0.x is not available at this time.

 

See

 Device configuration 

 What's new in IT Expert 

 

 

Requirements

 

FTP and/or SCP credentials for all the APC SNMP devices must be correctly configured in the Device File Transfer Settings option in the Gateway.

Note: SCP is supported in Gateway version 1.9.0 and newer.

 

Only the values exposed in the config.ini for both the source and destination device can be configured. User management settings may not be available on some devices.

Note: Device configuration is not supported for monitored NMC 4 devices. There is no config.ini file on NMC 4 devices.

 

About device settings

 

The list of device settings does not dynamically refresh. Device settings update during a discovery, a rediscovery, and after the FTP or SCP settings change as a result of a running device configuration on multiple devices or a Single device configuration. 

 

The date and time indicate when the device settings were most recently updated. 

Sensitive values, such as username, password, IP address, and location are masked. 

 

Configure devices

 

Select an APC SNMP device to use as the source to configure settings on other APC SNMP devices monitored by an EcoStruxure IT Gateway 1.5.0.x and greater.

IMPORTANT: Both the source device and the destination devices you want to configure must be monitored by the same Gateway.

 

  1. Log in to your ecostruxureit.com account.
  2. Click Device Configuration in the left sidebar. Click Begin.
  3. Choose the Gateway monitoring the devices you want to configure. 
    Both the source device and the destination devices you want to configure must be monitored by the same Gateway.
  4. Select the device you want to use as the source to configure settings on other devices. 
  5. Select the device settings you want to write to other devices.
  6. Select the destination devices you want to configuration settings on.
  7. Review your changes, and click Finish.

 

A progress bar shows the number of devices Completed, Failed, In progress, and Not started.

TIP: Filter, search, and sort to locate devices.

 

Get latest

Click to refresh the list of settings to be sure the latest settings are displayed. This list does not automatically refresh if a config change was made directly on the device.

 

Previous results list

Once configuration has finished, you can click Begin and click the Settings icon for any destination device to confirm that the settings were applied.

 

Also see Configure event actions for APC SNMP devices in IT Expert 

 

Troubleshooting device configuration failures

 

You can click Don't see the device you're looking for? in the Device Configuration wizard to see troubleshooting tips.

 

I can't find my device

The device you searched for isn't monitored by the Gateway you selected.

 

  1. Exit the Device Configuration wizard and click Begin.
  2. Select the Gateway that is monitoring the device you searched for. Both the source device for the template and the destination devices you want to configure must be monitored by the same Gateway.

 

There is no configuration for the device.

Make sure the FTP and/or SCP settings are configured correctly in the Device File Transfer Settings option of the Gateway.

 

  1. Log in to the Gateway that monitors the device.
  2. Verify the FTP and/or SCP settings.
  3. Rediscover the device. Note: You do not need to delete the device to rediscover it. Simply run a discovery again.

 

Results list

All destination devices that support config.ini are listed regardless of whether the settings from the source device are valid. Settings from the source device that are selected but cannot be applied are ignored.

 

Comm failed: Cannot communicate with the device. Check network settings and SNMP community names, and try again.

 

Invalid credentials: Check that the device credentials match the Device File Transfer Settings option of the Gateway.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.