Share Your Feedback – Help Us Improve Search on Community!
Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey
Configuring blade solutions
Search in
Improve your search experience:
Exact phrase→Use quotes " "(e.g., "error 404")
Wildcard→Use * for partial words(e.g., build*, *tion)
AND / OR→Combine keywords(e.g., login AND error, login OR sign‑in)
Keep it short→Use 2–3 relevant words, not full sentences
Filters→Narrow results by section(Knowledge Base, Users, Products)
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
You have entered an invalid email address. Please re-enter the email address.
This co-worker has already been invited to the Exchange portal. Please invite another co-worker.
Please enter email address
Send InviteCancel
Invitation Sent
Your invitation was sent.Thanks for sharing Exchange with your co-worker.
Valid blade configuration
The system ensures a valid configuration and guides you in placing blades in the bays of the blade enclosures based on the configured physical properties of the equipment.
Supported configurations
Any combination of full / half height with double / single width blades.
Amount
The system validates that there are a sufficient amount of bays available in the blade enclosure to contain the amount of bays that the blade servers take up.
Product family
If the blade enclosure has been specified to be of a certain brand or product family, only blades with the same properties can be placed in it. If there is no product family defined for the blade enclosure, only blades that have no product family defined either can be added to this enclosure.
Configuring blade solutions
Blade solutions are typically used when there is a need for high server density, power and cooling efficiency, and more flexible management functions than solutions with traditional servers provide. Blade servers are very compact servers. Many components have been removed to save space, minimize power consumption, and other considerations. Power and cooling supply is handled by the enclosure instead.
A blade enclosure can be mounted in a rack and contains a number of bays in which the blade servers (also referred to as blades) are placed. Bays and blade servers can be half-height or full-height, single-width or double-width.
The standard genome library installed with the application contains the most commonly used blade products. You can configure any additional blades and blade enclosures that you use, setting the number of bays and bay height and width (in any combination).
102237315_360037994594.png
123 Steps to...
Adding blade equipment to the rack layoutThe system guides you in placing the blade equipment in the rack layout. This ensures that blade enclosures fit into the rack and that blades fit into the enclosure bays.Before adding blade equipment to the layout, select Planning> Data Center in the Application bar and select to view a room in Rack Layout, for example by double-clicking a rack in the Floor Layout.
Drag the blade enclosure icon into the position in the rack layout that matches its position in the data center.
Drag the blade server icon into the position in the rack layout that matches its position in the data center. * Green highlights where you can place the equipment
Yellow highlights where you can place some of the equipment (the system will place what fits and leave out what does not fit)
Red highlights where you cannot place the equipment 3. Repeat above steps to add all blade equipment to the rack layout.
Tip
Tip: You can move or delete multiple items at the same time by using Ctrl-click or Shift-click.
4. Right-click the component icon and select Properties to e.g. define a custom name for it, or to use other menu options.