Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Xenta Programmable Daylight Savings Time settings incorrect

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Xenta Programmable Daylight Savings Time settings incorrect
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
2033 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Xenta Programmable Daylight Savings Time settings incorrect

Picard Product_Support
‎2018-09-07 07:42 AM

Last Updated: Crewman ContentModerator ‎2025-09-25 03:29 AM

Issue

The local time inside a Xenta programmable unit is dependent upon server time, time zone, and daylight savings time settings.  Incorrect DST settings result in incorrect times in the controller which causes problems from incorrect start times on HVAC equipment, to incorrect alarm time stamps in alarm queues.

Product Line

TAC Vista

Environment

  • Xenta Programmables version prior to 3.74
  • Xenta 280, 281, 282, 283, 300, 301, 302, 401, 401:B

Cause

In 2007, most of the United States and Canada changed when DST is observed to the second Sunday in March to the first Sunday in November.  Because it had never changed prior to that, programmable controllers retained the old settings (first Sunday in April to last Sunday in October).

Resolution

The issue was resolved with the release of firmware MOT version 3.74.  Upgrading your controllers to 3.74 is a viable solution, however not always cost effective.  There are two ways to work around the issue.

Note: For information on how to download firmware to Xenta programmable devices using the Download Wizard please see Download an .MOT file into a Xenta Programmable controller.

Configure TAC Xenta Central DST Settings

Refer to the TAC Vista Technical Manual Chapter 19.6

  1. In the folders pane, right-click the folder where you want to place the time event object.
  2. Point to New, point to Object, and then click Time Event – Object.
  3. Type the name.
  4. Open the time event object.
  5. On the General tab, type a description.
  6. On the Time Event Settings tab, set a suitable repeat interval, for example, first Monday in each week.
  7. Click OK.
  8. In the folders pane, right-click the folder where you want to place the Central Daylight Settings – Xenta object.
  9. Point to New, point to Object, and then click Central Daylight Settings – Xenta.
  10. Type the name.
  11. Open the Central Daylight Settings – Xenta object. Two options are available. You can use Windows start and end times for the daylight saving time or specify your own start and end times.
    If you want to specify your own start and end times:
    1. Clear the Use Windows settings check box.
    2. In the Daylight saving starts box, set the start time for the daylight saving time.
    3. In the Daylight saving ends box, set the end time for the daylight saving time.
  12. In the Update schedule box, browse to the time event object that triggers the push to the TAC Xenta devices.
  13. Click Select.
  14. Click OK.

Note: You must select Manual DST Mode and Central DST for each controller in the system for a global change to take effect.

Manually set DST Settings for each controller

The DST Xenta object is not available in all versions of Vista.  If that is not an option, DST settings on each controller can be manually set for the start day and stop day.  Unfortunately, time settings do not allow for designations of "first Sunday" or "last Sunday," only calendar dates.  So each controller will have to be edited each year to maintain correct time settings.

In order to facilitate this, this utility:  ODXentaTimezoneChanger was created.  It must be used each year to update the settings, but it will allow you to change all time settings on all controllers in a Vista database simultaneously, greatly reducing the time it takes to correct a system.

NOTE: If the Lonworks network has not been properly commissioned & downloaded the tree will not properly communicate with the Vista Server. Check your network tree for asterisks to see if any downloads are required.

Labels (1)
Labels:
  • TAC Vista
Attachments
ODXentaTimezoneChanger.zip
Tags (1)
  • Find more articles tagged with:
  • 4034
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.