Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Will Continuum work with SQL when it is configured with 64-bit ODBC drivers for the Database connection?

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Will Continuum work with SQL when it is configured with 64-bit ODBC drivers for the Database connection?
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • RobertAndriolo
    RobertAndriolo
  • Clifton_eakes
    Clifton_eakes
  • AdamSteele
    AdamSteele
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
2607 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Will Continuum work with SQL when it is configured with 64-bit ODBC drivers for the Database connection?

Picard Product_Support
‎2018-09-06 10:06 AM

Last Updated: Picard RobertAndriolo Picard ‎2022-03-11 01:58 PM

Issue

The SQL Server 2008 is running the 64-bit version as well as the Continuum Workstations are using 64-bit Operating Systems. In the interest of increasing the SQL access speeds can the ODBC connection between them also utilize the 64-bit ODBC driver?

Product Line

Andover Continuum

Environment

  • Continuum v1.94 (or greater)
  • Microsoft SQL Server 2008 64-bit
  • Microsoft SQL Server 2012 64-bit
  • Microsoft SQL Server 2014 64-bit
  • Microsoft SQL Server 2016 64-bit

Cause

Want to know if the SQL access speeds can be increased by taking advantage of using the 64-bit ODBC drivers.

Resolution

The Continuum application itself is a 32-bit application, this will require the 32-bit ODBC drivers to make a connection to the SQL Server. Even though we support Continuum in a 64-bit environment, it is still only a 32-bit application so the 32-bit ODBC drivers are used for the SQL connection.

Be aware that this is just the communications on the SQL side, the SQL application itself will still process data at 64-bit speeds if the 64-bit version is used.

Labels (1)
Labels:
  • Andover Continuum
Tags (3)
  • Find more articles tagged with:
  • 14243
  • CliftonEakes22
  • RobertAndriolo22
Was this article helpful? Yes No
0% helpful (0/1)
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.