Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

What type of cable should be used to wire inputs and outputs?

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • What type of cable should be used to wire inputs and outputs?
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • DavidFisher
    DavidFisher
  • PaulFr
    PaulFr
  • CraigEl
    CraigEl
  • sesa125819
    sesa125819
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
1 Like
6231 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

What type of cable should be used to wire inputs and outputs?

Picard Product_Support
‎2018-09-11 12:41 PM

Last Updated: Administrator CraigEl Administrator ‎2022-08-08 04:02 AM

Issue

What are the IO wiring requirements for the IO Modules?

Product Line

EcoStruxure Building Operation

Environment

  • Analogue, Digital, Input, Output
  • Cables
  • UI-16, DI-16, AO-8-x, AO-8-V-x
  • UI-8, DO
  • b3 Inputs

Cause

The existing documentation does not specify the exact cable types to be used.

Resolution

Different types of sensors can be used that come from different legacy systems, so cable types specified for the legacy systems will be appropriate for the same sensor type being connected to an Automation Server I/O module.

If you are using Xenta sensors with the 1.8K Ohm thermistors you should use the wiring rules as per the Xenta documentation. Of if you use Continuum 10K Ohm sensors, use the Continuum IO wiring rules etc.

Some suitable cables for most Analogue and Digital input, also analogue output applications are:

  • 18 AWG (16 x 30) 0.823 mm2 - single pair screened e.g. Belden 8760
  • 22 AWG (7 x 30) 0.325mm2 - single pair screened e.g. Belden 8761

The maximum distances that these cable can be run are dependent on the input requirements, for Temperature inputs this will depend on the temperature range and accuracy required.

For examples of of these cable distances see links below:

  • Continuum 10K Ohm sensors (also applicable for b3 controller inputs).
  • Xenta 1.8K Ohm sensors

For digital outputs cable should be used with appropriate size (current rating) to the loads being switched.

It is recommended to use screened cables and also ensure correct connections for analogue inputs as detailed in How to wire an Analog input to an IO Module.

Labels (1)
Labels:
  • EcoStruxure Building Operation
Attachments
Tags (1)
  • Find more articles tagged with:
  • 17781
Was this article helpful? Yes No
100% helpful (1/1)
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.