Issue
What is required to upgrade a UNC 196 outstation to a Sigma x96 controller?
Product Line
Satchwell BAS & SigmaEnvironment
- UNC 196
- UNC 296
- Sigma x96 Controller
- BAS 2000/2800(+)
Cause
Requirements to modernize BAS infrastructure by replacing legacy UNC 196 hardware with Sigma x96 components.
Resolution
To successfully upgrade the UNC 196 outstation to a Sigma x96 controller, the following components must be replaced:
- Comms/CPU Card
- Power Supply Card
These components are available as a bundled upgrade kit:
➡️ S-x96-UPKIT
Additional Consideration:
If the outstation includes a Maximum Demand Card, it must be replaced with a:
➡️ Digital Input Card (S-UNC-DI)
Notes:
- Ensure compatibility with existing BAS infrastructure before proceeding.
- Refer to Sigma documentation for installation and configuration details.