Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Vista lock-up caused by tacldv32.dll crash

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Vista lock-up caused by tacldv32.dll crash
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • DavidFisher
    DavidFisher
  • Benji
    Benji
  • CraigEl
    CraigEl
  • Sacco
    Sacco
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
1984 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Vista lock-up caused by tacldv32.dll crash

Picard Product_Support
‎2018-09-10 01:13 PM

Last Updated: Administrator CraigEl Administrator ‎2022-08-09 08:49 PM

Issue

Vista locks up randomly and displays application crashes. Investigating the Windows Event log shows the following errors pointing to tacldv32.dll. For more information on Windows Event Log, see Viewing, Saving, Sharing Windows Event Logs for Troubleshooting Purposes.

Faulting application tacos.exe, version 0.1.0.0, faulting module tacldv32.dll, version 1.0.0.1, fault address 0x00007310

Product Line

TAC Vista

Environment

  • Vista Server
  • LNS Communication Port
  • Large LNS network, or many smaller LNS networks
  • Orion Stack

Cause

The DLL file, tacldv32.dll, is responsible for managing communications through an LNS communication port. If that is being overwhelmed with information from too many devices on the port, this DLL will crash.

If the number of networks is only one and the database size is reasonable then the problem can be caused by a corrupted and non functioning LNS database.See Also Echelon LNS Utilities LNS Database Validator.

Resolution

If the number of networks is high then LNS communication must be managed by an Orion Stack, or NIC-852. This does not utilize tacldv32.dll and will stop the application crashes.

If the number of networks is low, but the size of the networks is quite large, then it is also advisable to allow the Orion Stack to manage communication and will prevent the application crashes.

If the number of networks is low and they are not very sizeable, then ensure that LNS database is working properly independently of Vista Server. If it has problems, investigate the LNS problems further, looking for any errors that can be searched on other articles.

*Note that if you receive the tacldv32.dll error and are currently using an Orion Stack or NIC-852. There is a problem with the Orion Stack or NIC-852 installation or configuration.

Hovering the mouse over the Communication Port objects in the TAC Vista Workstation should produce a pop-up window stating "Loytec Port". If it says "LNS Port", there will still be a need for using tacldv32.dll resource.

Labels (1)
Labels:
  • TAC Vista
Tags (1)
  • Find more articles tagged with:
  • 5328
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.