Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Various SQL Errors received during a database restore

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Various SQL Errors received during a database restore
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • DavidFisher
    DavidFisher
  • Product_Support
    Product_Support
  • RobertAndriolo
    RobertAndriolo
  • CraigEl
    CraigEl

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
3640 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Various SQL Errors received during a database restore

Picard Product_Support
‎2018-09-06 01:39 PM

Last Updated: Administrator CraigEl Administrator ‎2022-08-08 06:03 PM

Issue

Receive the following errors when trying to restore a SQL database:

ERROR MESSAGE #1
Msg 3169, Level 16, State 1, Line 1
The database was backed up on a server running version 10.50.1600. That version is incompatible with this server, which is running version 10.00.1600. Either restore the database on a server that supports the backup, or use a backup that is compatible with this server.
Msg 3013, Level 16, State 1, Line 1
RESTORE DATABASE is terminating abnormally.

ERROR MESSAGE #2
Server: Msg 3241, Level 16, State 7, Line 1
The media family on device [path of backup] is incorrectly formed. SQL Server cannot process this media family.
Server: Msg 3013, Level 16, State 1, Line 1
RESTORE DATABASE is terminating abnormally.

ERROR MESSAGE #3
Server: Msg 3169, Level 16, State 1, Line 1
The backed-up database has on-disk structure version 661. The server supports version 539 and cannot restore or upgrade this database.
Server: Msg 3013, Level 16, State 1, Line 1
RESTORE DATABASE is terminating abnormally.

ERROR MESSAGE #4
Server: Msg 3241, Level 16, State 7, Line 1
The media family on device [path of backup] is incorrectly formed. SQL Server cannot process this media family.
Server: Msg 3013, Level 16, State 1, Line 1
RESTORE DATABASE is terminating abnormally.

ERROR MESSAGE #5
Server: Msg 3169, Level 16, State 1, Line 1
The backed-up database has on-disk structure version 655. The server supports version 539 and cannot restore or upgrade this database.
Server: Msg 3013, Level 16, State 1, Line 1
RESTORE DATABASE is terminating abnormally.

ERROR MESSAGE #6
Server: Msg 3169, Level 16, State 1, Line 1
The backed-up database has on-disk structure version 611. The server supports version 539 and cannot restore or upgrade this database.
Server: Msg 3013, Level 16, State 1, Line 1
RESTORE DATABASE is terminating abnormally.

Product Line

Other, TAC INET, TAC Vista

Environment

  • SQL Server 2008, SQL Server 2005 and SQL Server 2000
  • Enterprise, Standard, Express, MSDE

Cause

You cannot restore a backup created with a newer version of SQL Server on an instance running an older version of SQL Server. Unfortunately, the error messages that are displayed may not always tell you that it is a versioning problem. Here are various combinations of SQL versions and there associated error messages:

SQL Server 2008 R2 to SQL Server 2008
Msg 3169, Level 16, State 1, Line 1
The database was backed up on a server running version 10.50.1600. That version is incompatible with this server, which is running version 10.00.1600. Either restore the database on a server that supports the backup, or use a backup that is compatible with this server.
Msg 3013, Level 16, State 1, Line 1
RESTORE DATABASE is terminating abnormally.

SQL Server 2008 R2 to SQL Server 2005
Server: Msg 3241, Level 16, State 7, Line 1
The media family on device [path of backup] is incorrectly formed. SQL Server cannot process this media family.
Server: Msg 3013, Level 16, State 1, Line 1
RESTORE DATABASE is terminating abnormally.

SQL Server 2008 R2 to SQL Server 2000
Server: Msg 3169, Level 16, State 1, Line 1
The backed-up database has on-disk structure version 661. The server supports version 539 and cannot restore or upgrade this database.
Server: Msg 3013, Level 16, State 1, Line 1
RESTORE DATABASE is terminating abnormally.

SQL Server 2008 to SQL Server 2005
Server: Msg 3241, Level 16, State 7, Line 1
The media family on device [path of backup] is incorrectly formed. SQL Server cannot process this media family.
Server: Msg 3013, Level 16, State 1, Line 1
RESTORE DATABASE is terminating abnormally.

SQL Server 2008 to SQL Server 2000
Server: Msg 3169, Level 16, State 1, Line 1
The backed-up database has on-disk structure version 655. The server supports version 539 and cannot restore or upgrade this database.
Server: Msg 3013, Level 16, State 1, Line 1
RESTORE DATABASE is terminating abnormally.

SQL Server 2005 to SQL Server 2000
Server: Msg 3169, Level 16, State 1, Line 1
The backed-up database has on-disk structure version 611. The server supports version 539 and cannot restore or upgrade this database.
Server: Msg 3013, Level 16, State 1, Line 1
RESTORE DATABASE is terminating abnormally.

Resolution

Possibly the quickest and simplest solution may be to uninstall any software including SQL currently installed, then re-install any software along with the correct version of SQL. If this is not an option, then Microsoft does provide information on how to upgrade different versions of SQL. Links are provided below:

  • How to: Upgrade to SQL Server 2005 (Setup)
  • How to: Upgrade to SQL Server 2008 (Setup)

Also check Software and Firmware compatibility matrix for older versions of the traditional product lines for supported Operating Systems and SQL versions.

Labels (2)
Labels:
  • TAC INET
  • TAC Vista
Tags (1)
  • Find more articles tagged with:
  • 5679
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.