Join our 30-minute expert session on July 10, 2025 (9:00 AM & 5:00 PM CET), to explore Digital Twins, cooling simulations, and IT infrastructure modeling. Learn how to boost resiliency and plan power capacity effectively. Register now to secure your spot!

Valid access events are not logging or showing in the active event view but Invalid events show

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Valid access events are not logging or showing in the active event view but Invalid events show
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • David_Kendrick
    David_Kendrick
  • Alan_Wood
    Alan_Wood
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
2480 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Valid access events are not logging or showing in the active event view but Invalid events show

Picard Product_Support
‎2018-09-10 05:23 AM

Last Updated: Admiral David_Kendrick Admiral ‎2023-06-20 07:31 AM

Issue

On a working system, valid access events no longer show in the active event view and are no longer visible in the accessevent table within the Database.   However, invalid events continue to work normally. 

Product Line

Andover Continuum

Environment

  • Access Events
  • Logging

Cause

An incomplete object may have been added to the Continuum Database recently that is interfering with queries running against that database.

Resolution

Try the following steps to troubleshoot the issue

  1. Does the issue happen on multiple CyberStations?
  2. Ensure all the event types are selected in the active event view that is being used on the door(s).
  3. Perform a CyberStation Teach

    It is best to contact PSS and work with them at this point with the following procedures.
     
  4. Verify that access events are being sent from the controller to the CyberStation using Wireshark.
  5. Verify that the issue follows the Database by loading the database in a test environment to see if the issue still happens. 
  6. On the TEST database, use SQL Management Studio:
    1.  SQL Query: set acdbversion=0  (execute the query)
    2.  Update database: launch Database Initialization Server/Stand Alone
  7. Enter sa password and update database
  8. Restore database or locate incomplete object
    1. The quickest fix would be to revert to a known good database. Once restored, the events in the controllers would be downloaded to the database.
    2. Finding the object in the database that has caused the issue can be very challenging. Check to see if there was a controller recently added and if the issue began to happen after that. If for some reason a controller had been added and it wasn't completed normally then it could cause this issue.
    3. Check to see if there is a controller in the InfinityController table with an objectidhi or objectidlo with a zero value. If so, delete that controller and see if the valid access events start coming in.

It may also be necessary to use the SQL profiler to view the entries that are being made into the database. See the following link  below for  more information. http://msdn.microsoft.com/en-us/library/ms181091.aspx

 

NOTE:

Turning off the Primary and Secondary Access Server will cause the access events to buffer in the controllers, so that these events will be inserted into the database once valid access event logging has been restored. After turning off the primary and secondary, check the Access Log infinity system variable on the controllers. If they are non zero values, then events are buffering. There is a limited amount of access events that can be stored in the controllers before loss of data occurs.

Labels (1)
Labels:
  • Andover Continuum
Tags (2)
  • Find more articles tagged with:
  • 7059
  • DavidKendrick23
Was this article helpful? Yes No
No ratings

Link copied. Please paste this link to share this article on your social media post.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.