Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

The procedure to follow for upgrading or downgrading the I/A Series G3 software in an I/A Series ENC

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • The procedure to follow for upgrading or downgrading the I/A Series G3 software in an I/A Series ENC
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • Ramaaly
    Ramaaly
  • Product_Support
    Product_Support
  • sesa116868
    sesa116868

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
6272 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

The procedure to follow for upgrading or downgrading the I/A Series G3 software in an I/A Series ENC

Picard Product_Support
‎2018-09-10 09:04 PM

Last Updated: Administrator CraigEl Administrator ‎2023-03-30 05:51 PM

Issue

What is the procedure for upgrading the I/A Series G3 software in an I/A Series ENC?

Product Line

TAC IA Series

Environment

  • I/A Series G3 Workbench software on computer (both the old version and new version need to be installed on the computer)
  • I/A Series G3 ENC-520 or ENC-410

Cause

Need to upgrade the software that is installed in the ENC.

Resolution

  1. With the old version of Workbench running on the computer, backup the station running in the ENC.  All required graphic files, etc., stored in the ENC should also be backed up.  Note the station folder name for use in step 5, below.
  2. Verify that the license in the ENC is compatible with the new release to be installed. If not, use the License Manager (under the Platform) to install an updated license. If the correct version of the license is not currently available, it must be obtained and installed prior to beginning step 6, below.
  3. If the new release of the I/A Series G3 software has not already been installed on the computer, install it now.
  4. Verify that the Workbench computer has a license that is version compatible with the new release of the I/A Series software to be installed.  If the license is not version compatible, acquire a new license for the Workbench computer before continuing.
  5. Copy the entire named station folder (used in step 1) from the old release Stations folder to the new release Stations folder.  See NOTE below regarding the installation of a version downgrade.
  6. Run the "Install Platform Daemon" command from the Windows Start Menu folder for the new version of the software.
  7. Open the Workbench in the new version of the I/A Series G3 software and connect to the platform of the ENC to be upgraded.
  8. From the Platform menu, open the License Manager and verify that the ENC license has been updated to allow use with the new version of the I/A Series G3 software.
  9. Right-Click on the ENC platform in the Workbench tree and select Commissioning Wizard.
  10. Complete the commissioning process as documented in the Niagara AX Install and Startup Guide .
    • On the first screen, select the operations to be performed.  The required minimum operations will normally be checked and shown in grey.  The "Install a station..." option needs to be checked if not already checked.
    • Click [Next] to begin the commissioning process. 
    • Continue through the various steps, as required.  
    • When prompted, select the station copied in step 5.
    • When prompted, verify that all required modules are available and are selected for installation.
    • Allow the commissioning process to complete, following the prompts as required.
  11. The upgrade is now complete.  Start the station as required.

NOTE: Do not use the process to directly downgrade the version of software installed in an ENC.  You must use the Platform "Distribution File Installer" to install the appropriate clean distribution (from the cleanDist folder under the software version to be installed.  Typically, only one clean distribution file will be available to be installed.  Select that file then click the [-> Install] button to downgrade the ENC software.  This process needs to be done as noted in step 5, above, after backing up the station but before beginning the commissioning of the device with the older I/A Series G3 software version.

Labels (1)
Labels:
  • TAC IA Series
Attachments
Tags (2)
  • Find more articles tagged with:
  • 7795
  • RamaAly23
Was this article helpful? Yes No
100% helpful (2/2)
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.