Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

TAC Xenta Server SNMP settings - Changing and disabling

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • TAC Xenta Server SNMP settings - Changing and disabling
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
1757 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

TAC Xenta Server SNMP settings - Changing and disabling

Picard Product_Support
‎2018-09-11 01:00 PM

Last Updated: Crewman ContentModerator ‎2025-09-01 03:36 AM

Issue

There is no clear guidance on how to handle the SNMP settings for TAC Xenta Servers

Product Line

TAC Vista

Environment

  • TAC Xenta Server
  • TAC XBuilder
  • SNMP

Warning

Potential for Data Loss: The steps detailed in the resolution of this article may result in a loss of critical data if not performed properly. Before beginning these steps, make sure all important data is backed up in the event of data loss. If you are unsure or unfamiliar with any complex steps detailed in this article, please contact Product Support Services for assistance.

Cause

Previously the SNMP feature has not been widely used and has not been a security concern.

There are two types or flavors of SNMP. One is for browsing a device to get information about it (SNMP Agent), and the other is to automatically send alarms from a given device to a central alarm system (SNMP Alarm Trap).

Now according to reports from the field, IT departments are starting to get concerned about the SNMP feature in Xenta Servers. A general overview of how SNMP can be used maliciously for intrusion can be studied here.

Normally the IT department requests that:

  1. The default community string is changed
  2. SNMP is disabled

Here is an example of what you see when you browse a Xenta Server (having the correct Xenta Server mib file) using a SNMP browser such as "MIB Browser" from iReasoning

Here is an example of alarms received from a Xenta Server via SNMP

Resolution

All (or most) SNMP settings are changed through TAC XBuilder

First step is to change the default community name. If the community name is either "private" or "public" (the latter is default), it can be browsed without knowing the name. You simply change the name in "Community Name" and "Trap Community Name". Download all project files to the Xenta Server afterwards.

Now when you try to browse the Xenta Server from the SNMP agent without first defining the community name, you will not be able to retrieve data.

Next, we can disable the SNMP Alarm Trap. Download all project files to the Xenta Server afterwards. After that, alarms will not be sent to the IP address configured.


Following here are advanced steps to change the ports used for SNMP (161 and 162)


If the settings described above are not enough, we can change the port number used for SNMP. This is however a little more complicated. You need to connect to the Xenta Server using FTP (Note that the FTP access may be disabled, refer to Disable FTP in the Xenta 5/7/9xx Controllers if unsure how to enable this), and fetch the following file: /sys/system/snmp.cfg

  1. Open the file in Notepad
  2. Change the two port number as below - you can choose other port numbers, but it is crucial that they are not the same as any other ports used by the Xenta Server.
  3. Upload the changed file to the same location on the Xenta Server
  4. Download the project from TAC XBuilder, choosing to download all files
  5. You now get this message
  6. Here you must click "Target system" or the changed settings are overwritten
  7. Note that the port numbers defined in XBuilder have not changed yet
  8. Save the project and close XBuilder
  9. Open the project again
  10. You will now see that the port numbers have the value you defined in the file earlier
  11. Now when you try browsing the Xenta Server with a SNMP tool, you can no longer connect on the default port 161
Labels (1)
Labels:
  • TAC Vista
Attachments
tacXentaMibFiles.zip
Tags (1)
  • Find more articles tagged with:
  • 17547
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.