Issue
Can the Sigma Web Client be used effectively on Apple mobile devices such as iPads and iPhones?
Product Line
Satchwell BAS & SigmaEnvironment
- Sigma Web Client
- iPhone
- iPad
Cause
Apple mobile devices (iPhone and iPad) do not support ActiveX components, which are required for rendering Sigma Web Graphics.
Resolution
Due to the lack of ActiveX support on iOS devices:
- Sigma Web Graphics will not function properly on iPads or iPhones.
- Users should access the Sigma Web Client from a Windows-based device with a compatible browser that supports ActiveX (e.g., Internet Explorer).
Additional Notes
- This limitation applies to all iOS versions and is not specific to a particular model or software update.
- Android devices may also face similar limitations depending on browser compatibility and support for Active