Issue
Clarification needed on the correct configuration of jumpers for the Analogue Input (AI) card.
Product Line
Satchwell BAS & SigmaEnvironment
Sigma Analogue Input (AI) Cards
Cause
Users may be unsure how to correctly configure jumpers on the AI card to support different input types.
Resolution
The jumper configuration on the Sigma Analogue Input card supports three types of inputs:
- Resistance
- Voltage
- Current
Each input type requires a specific jumper setting. Refer to the screenshot below for visual guidance on jumper positions.
Tip: Ensure the jumper settings match the sensor type connected to the input channel to avoid incorrect readings.