Issue
A customer needs a small number of I/O points at the location of the Integration Controller and wants to know if Sigma Integration Controllers support onboard I/O.
Product Line
Satchwell BAS & SigmaEnvironment
Sigma Integration Controllers
Cause
The customer is evaluating the feasibility of using an Integration Controller (IC) to handle limited I/O requirements locally, without deploying additional hardware.
Resolution
The IC3 Integration Controller does not have any onboard I/O capabilities.
Therefore, it cannot be used in applications where direct I/O is required at the controller location.