Issue
Users need to interpret the Diagnostic LED indicators on various UNC controllers and DNN modules to assess device status and troubleshoot effectively.
Product Line
Satchwell BAS & SigmaEnvironment
- Sigma
- Devices
- Controllers
- UNC X96
- UNC 532
- DNN3
Cause
Diagnostic LEDs are designed to provide visual feedback on the operational status of the controller. Misinterpretation or lack of documentation can lead to confusion during diagnostics.
Resolution
Refer to the following LED behavior chart to understand the controller's current state: