Issue
How to enable or disable Contingency Logging in Sigma.
Product Line
Satchwell BAS & SigmaEnvironment
Satchwell Sigma
Cause
Users may be unsure when and how Contingency Logging is activated or deactivated for Sigma objects.
Resolution
Default Behavior
- When a new Sigma object is created, Contingency Logging is enabled automatically.
Disabling Contingency Logging
- Ensure the controller is online and connected to the Sigma server.
- Open System Manager.
- Navigate to the Logging menu and select Contingency Setup
.
- In the dialog box:
- Uncheck Enable to deselect Contingency Logging.
- Click OK to confirm.
- Contingency Logging is now disabled for the selected object.
Enabling Contingency Logging
- Follow the same steps as above to access the Contingency Setup dialog.
- In the dialog box:
- Click Enable to activate Contingency Logging.
- The Entries and Interval fields will become available.
- Note: The number of entries shown is the maximum allowed for the selected interval. Do not exceed this value.
- Click OK to complete the process.
- Click Enable to activate Contingency Logging.
- Contingency Logging is now enabled for the object.