Issue
After upgrading to Sigma 4.08, the Sigma server (SigmaSvr.exe) fails to start. An error message may be displayed.
Product Line
Satchwell BAS & SigmaEnvironment
Sigma 4.08 Build 3.46.57
Cause
The issue occurs due to the absence of a valid licensing method on the Sigma server following the upgrade from Sigma 4.04.
Resolution
Resolution
To resolve this issue, ensure that one of the following valid licensing methods is available:
- A valid Sigma dongle is connected to the server.
- The StruxureWare Building Operation License Administrator software is installed, along with a valid license.
Additional Notes
- This issue is specific to Sigma 4.08 Build 3.46.57.
- If licensing is correctly configured and the issue persists, contact support for further assistance.