Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

RP-C Modbus Usage with 64-Bit Registers and Multiple Ports

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • RP-C Modbus Usage with 64-Bit Registers and Multiple Ports
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • RobertAndriolo
    RobertAndriolo
  • PeterLarsen
    PeterLarsen

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
4504 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

RP-C Modbus Usage with 64-Bit Registers and Multiple Ports

PeterLarsen Champion
‎2023-12-07 02:11 PM

Last Updated: CraigEl Champion ‎2023-12-10 06:24 PM

 

Issue

  1. How are Modbus 64-bit registers calculated in the Modbus limitations on an RP-C?
  2. Can both RS485 ports be used for Modbus on an RP-C?

Product Line

EcoStruxure Building Operation

Environment

  • SpaceLogic RP Controller series
  • RP-C Modbus

Cause

  1. EBO version 2023 introduced 64-bit register support in RP controllers. EBO Webhelp states that an RP-C has a maximum limit of 250 Modbus registers. It is unclear if a 64-bit register is counted as four 16-bit registers or just one register on the Modbus maximum count.
  2. The RP-C controller has two RS-485 ports, and it is unclear if both ports can be utilized for Modbus simultaneously.

Resolution

  1. A 64-bit Modbus register is counted as one register in the Modbus maximum register count.
  2. The RP-C controller has two configurable RS-485 ports that can be used for:
    • Sensor bus
    • Room bus
    • Modbus network

    As per EBO webhelp, the controller can host two networks, but only one network of each network type.

Labels (1)
Labels:
  • EcoStruxure Building Operation
Tags (1)
  • Find more articles tagged with:
  • PeterLarsen23
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.