Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

OEM Conversions

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • OEM Conversions
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • RandyDavis
    RandyDavis
  • JonGreen
    JonGreen
  • StevenTurney
    StevenTurney

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
1940 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

OEM Conversions

Commander JonGreen Commander
‎2022-04-26 01:12 PM

on ‎2022-04-26 01:12 PM

Issue

OEM conversions allow for a non-Access Expert/Feenics Mercury board to be converted to an Access Expert board. This is only applicable to the IP level controllers and the AX-OEMC codes are not needed for the downstream controllers.  The process will change the OEM code within the Device info page of the controller. This allows the board to receive the correct firmware and operate within Access Expert. 

Product Line

EcoStruxure Access Expert

Environment

Access Expert Controller

Cause

Not all controller boards are compatible with Access Expert by default

Resolution

To perform the OEM conversion on an intelligent controller, an AX-OEMC code is needed per IP Controller connected to your system.  These are ordered through iPortal and will require some specific information from the customer's site.  With your order, please include (both are located on the white sticker located on the actual controller:

  • Model of controller
  • Serial number
  • Email address for recipient

The OEM flash code will be emailed to the person whose email address is used in the order as the recipient. 

To convert the controller:

Using IP Server.

  1. Connect directly to the controller with an ethernet cable
  2. Locate the IP address of the controller (The default IP address can also be used).
  3. Go to the 'Host Comm' section of the configuration manager.
  4. Set the connection type to 'IP Server'. Take note of the Port
  5. Data Security should be set to none or TLS if Available
  6. Save and apply changes.
  7. Open the OEM & firmware utility. Download Here
  8. Set the controller connection type of the utility to 'Server'.
  9. Enter the MAC address of the controller.
  10. Enter the IP address of the controller.
  11. Enter the TCP port used by the controller.
  12. Select 'Connect'.
  13. Once connected, enter the Authorization code provided by Schneider Electric.
  14. Select 'Convert'.
     

    Conversion complete.png

  15. OEM conversion complete.

Once the conversion has been completed, the panel will need to be set back to the IP client to connect to the Access Expert Mercury Communication Servers. See the Configuring Controllers for IP Client page for instructions.  

Labels (1)
Labels:
  • EcoStruxure Access Expert
Tags (1)
  • Find more articles tagged with:
  • JonGreen22
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.