Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Not possible for BACnet alarm to trigger directly on a variable from a Function Block Program

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Not possible for BACnet alarm to trigger directly on a variable from a Function Block Program
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • Ramaaly
    Ramaaly
  • Product_Support
    Product_Support
  • sesa139513
    sesa139513
  • DavidFisher
    DavidFisher
  • HenrikTarpgaard
    HenrikTarpgaard

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
2743 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Not possible for BACnet alarm to trigger directly on a variable from a Function Block Program

Picard Product_Support
‎2018-09-06 10:42 AM

Last Updated: Administrator CraigEl Administrator ‎2023-03-29 04:48 PM

Issue

Unable to have BACnet alarm trigger directly on a variable from a Function Block Program

Product Line

EcoStruxure Building Operation

Environment

Building Operation Automation Server

Cause

Building Operation does not have the possibility for a BACnet alarm to directly monitor a variable from a Function Block Program.  The problem with doing this is that a Function Block Program is not a BACnet visible object (a BACnet client cannot see it, even as a proprietary object type), and we do not see any provision in the BACnet standard for an alarm object to reference something not visible to BACnet.

Resolution

The workaround is to create a BACnet point (a BACnet Value object would make the most sense), and bind it to the Function Block Program variable.

 

There is however an option which may avoid "double" work.  In Building Operation we have implemented intrinsic alarming on the BACnet points and values.  This means that the point can detect and report alarms without creating a separate alarm object.  (they still need to reference to a BACnet notification class just like normal BACnet alarm objects).

 

The only limitation is in the choice of algorithm:

  • Analog objects (Input, output, Value) support the out-of-range algorithm (high-limit, low-limit).
  • Digital and Multistate objects* (input, and value) support the change-of-state algorithm.

*In Building Operation, we do not have digital or multi-state outputs with alarming, because we do not support "command-failure" type alarm that those require.

Labels (1)
Labels:
  • EcoStruxure Building Operation
Tags (2)
  • Find more articles tagged with:
  • 12331
  • RamaAly23
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.