Issue
Product Line
TAC IA Series
Environment
- Niagara R2
- ProView display
Cause
Resolution
Ensure the following JAR files are installed in the UNC:
lonDistech-2.307.529.v1.jarlonDistechWizards-2.306.515.v111.jarwizard-2.301.529.v1.jarlonworks-2.301.529.v1.jar
Additional Notes:
- These files must match the Niagara R2 version for compatibility.
- Refer to the Niagara R2 documentation for steps to install JAR files in the UNC.