Issue
Clarification is needed on how to correctly wire and connect Micronet LCDs to various Satchwell MicroNet controllers.
Product Line
Satchwell MicroNet
Environment
- Micronet LCD / Micronet 50 series LCD
- Micronet 300 / 350 series controllers
- Micronet 440 / 450 series controllers
- Micronet 500 / 550 series controllers
- Micronet 620 / 650 series controllers
Cause
Micronet LCDs have multiple wiring and connection options depending on:
- The specific controller model in use
- Communication type (e.g., direct, networked)
- Installation method (e.g., panel mount, wall mount)
This variability can lead to confusion or miswiring during installation or maintenance.
Resolution
Refer to the Micronet LCD Connections document (updated July 2012), which provides a comprehensive summary of connection options for Micronet LCDs across different controller models.
📎 Attachment: MN LCD connections (updated July 2012).pdf
This document includes:
- Wiring diagrams
- Supported controller models
- Communication interface details
- Installation best practices
Ensure that:
- The correct controller model is identified before wiring
- Communication settings (e.g., bit switch configurations) are verified
- Power supply requirements (e.g., 24VDC) are met