Join our 30-minute expert session on July 10, 2025 (9:00 AM & 5:00 PM CET), to explore Digital Twins, cooling simulations, and IT infrastructure modeling. Learn how to boost resiliency and plan power capacity effectively. Register now to secure your spot!

Installing and Running an IC-Gen OPC on Windows 7 64 bit OS

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Installing and Running an IC-Gen OPC on Windows 7 64 bit OS
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • DavidFisher
    DavidFisher
  • sesa139513
    sesa139513
  • CraigEl
    CraigEl
  • RogerHa
    RogerHa
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
1320 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Installing and Running an IC-Gen OPC on Windows 7 64 bit OS

Picard Product_Support
‎2018-09-11 04:23 AM

Last Updated: Administrator CraigEl Administrator ‎2022-08-10 05:15 PM

Issue

Installing the Sigma IC-Gen on unsupported OS Platforms

Product Line

Satchwell Sigma

Environment

Sigma IC-Gen and Windows 7

Cause

Customers have the IC-Gen already installed on sites. The PC's/Server are now being upgraded and the supported OS are not generally available.

Resolution

Some basic testing using IC-Gen OPC software loaded onto a Windows 7 64 bit PC has been carried out. The software installs with no issues into the default locations.

The SigmaSvr can be run as a service as is it designed to do, but in this configuration no icon appears on the task bar, hence the status of the IC cannot been viewed at any time, although it is running and can be viewed as normal from the main Sigma server.

It is recommended that it is run as an application. This is done as described in Running Sigma server as an application There is a minor issue with closing the program. It can only be achieved using the task manager and performing an "End Task."

Testing has been carried out using the IC-Gen on the OPC platform. Only basic functionality was tested. An OPC simulator was used to generate values for the IO objects. Program objects where also used. Alarms and Logging were also setup and worked as expected.

The IC appeared to work correctly on the OS platform, but it has not been fully tested and is not supported in this configuration. Support in the event of a failure will be limited to basic operations. No capacity testing has been done so actual IO performance cannot be specified.

Labels (1)
Labels:
  • Satchwell BAS & Sigma
Tags (1)
  • Find more articles tagged with:
  • 12812
Was this article helpful? Yes No
No ratings

Link copied. Please paste this link to share this article on your social media post.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.