Join our 30-minute expert session on July 10, 2025 (9:00 AM & 5:00 PM CET), to explore Digital Twins, cooling simulations, and IT infrastructure modeling. Learn how to boost resiliency and plan power capacity effectively. Register now to secure your spot!

How to integrate I/NET with Pelco Analog Matrix

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • How to integrate I/NET with Pelco Analog Matrix
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • DavidFisher
    DavidFisher
  • CraigEl
    CraigEl
  • sesa145087_brid
    sesa145087_brid
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
3872 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

How to integrate I/NET with Pelco Analog Matrix

Picard Product_Support
‎2018-09-10 10:17 PM

Last Updated: Administrator CraigEl Administrator ‎2022-08-09 09:40 PM

Issue

How to integrate I/NET with Pelco Analog Matrix in order to implement some features, such as:

  • Switch specific camera image to specific monitor.
  • Switch specific camera to specific preset and display it on specific monitor.

Product Line

TAC INET

Environment

  • I/NET
  • Pelco CCTV system
  • Pelco Matrix

Cause

In some projects there is demand for access control system to integrate with analog CCTV system to do the alarm interaction. I/NET can integrate with Pelco CCTV system with ASCII code communication.

Resolution

I/NET communicates with Pelco analog CCTV system through ASCII code. There are two kinds of communication port for Pelco matrix, which are RS232 and RS485/422. For RS232 port for matrix, an RS232 to RS 232 cable is needed. If there are no COM ports for computer, an USB to RS232 converter is needed. For RS485/422 port for matrix, an RS232 to RS485/RS422 converter or USB to RS485/422 converter is needed. Connect the I/NET server to Pelco matrix through this converter, and the steps below should be followed:

  1. Open the I/O Configuration of I/NET, and choose the port for text output port and baud rate for the port communicating.


  2. In the AMT, choose Edit--->Text Library, and click Add.
  3. Choose a point for alarm interaction, and the status of the point to activate the interaction: alarm, acknowledge, return to normal (RTN) and acknowledged/return to normal (RTN).


  4. In the text area, enter the ASCII code for matrix. For the two applications of the alarm interaction, different ASCII code should used:
    • 1Ma1#a, which means switching 1# camera image to 1# monitor
    • 1Ma7#a1\\a, which means switching 7# camera to 1# preset and display it on 1# monitor. Here "\a" is an escape sequences for I/NET, so we need one more "\".

Then the integration with I/NET and Pelco CCTV system is finished. When the specific point goes into alarm, then the specific camera can be switched to specific preset and displayed on specific monitor.

For more applications of the integration with Pelco analog matrix, refer to the documentation for the Pelco ASCII Protocol Manual.

And for more information about how to set text output in I/NET, refer to Text Output through RS-232 Port in I/NET.

Labels (1)
Labels:
  • TAC INET
Attachments
Tags (2)
  • Find more articles tagged with:
  • 8344
  • inet
Was this article helpful? Yes No
No ratings

Link copied. Please paste this link to share this article on your social media post.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.