Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

How to create a Binary Input or Digital Input on a MPM controller

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • How to create a Binary Input or Digital Input on a MPM controller
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • MaximeLaudren
    MaximeLaudren
  • sesa139513
    sesa139513
  • SaidSawan
    SaidSawan
  • DavidChild
    DavidChild
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
2341 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

How to create a Binary Input or Digital Input on a MPM controller

Product_Support
‎2018-09-06 09:49 AM

Last Updated: MaximeLaudren Mentor ‎2022-08-18 09:33 AM

Issue

How to create a Binary Input or Digital Input on a MPM controller

Product Line

EcoStruxure Building Expert

Environment

SmartStruxure Lite Multi-Purpose Manager (MPM)

Cause

When a Binary Input is created, the object does not work.

There is no documentation on how to create a Binary Input

Resolution

In order to use a Binary Input, both the BI object and the corresponding Analog Input AI object must be added from the object list. For example, if you need to use BI3 with a dry contact, you will also need to add AI3 and toggle its "input type" to Ohms, then save the object. You also need to keep the object in the object list.

With regards to “Input type” for the Binary Inputs: (the "input type" property is in the AI object)

-When set in Volts, anything >= 2VDC will be considered a 1 status.
                                   anything < 2VDC will be conspired a 0 status.

-When set in Ohms, anything < 10kOhm will be considered a 1 status.
                                     anything >= 10KOhm will be considered a 0 status.

Note: When "Input type" is set to ohms, a dry contact must be used for the BI to work properly. BO1 and BO2 of the MPM can be used for example, but not the relays of the TE2 as they are not dry contacts by design.

Labels (1)
Labels:
  • EcoStruxure Building Expert
Tags (5)
  • Find more articles tagged with:
  • 15152
  • analogue
  • MaximeLaudren22
  • mpm-gw
  • mpm-un
Was this article helpful? Yes No
100% helpful (1/1)
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.