Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Flash upgrade an offline Continuum controller

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Flash upgrade an offline Continuum controller
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • PaulFr
    PaulFr
  • DavidFisher
    DavidFisher
  • BillNeville
    BillNeville
  • CraigEl
    CraigEl
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
3514 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Flash upgrade an offline Continuum controller

Picard Product_Support
‎2018-09-10 05:09 AM

Last Updated: PaulFr Schneider Alumni (Retired) ‎2022-08-18 03:39 AM

Issue

A network level controller is shown offline. Can a flash upgrade (Update OS) be done to it?

Product Line

Andover Continuum

Environment

  • BCX
  • ACX5720 ACX5740
  • NC2
  • CX9900

Cause

A bCX needed a flash upgrade but was offline in CyberStation. How can we update the OS?

Resolution

The Update OS function can sometimes be completed even if the controller indicates that it is offline.

If it cannot be pinged from CyberStation, it will not likely be able to be upgraded in its current state and may require returning for repair.

But if it can be pinged it, try doing the Update OS.

Follow the progress in the Distribution window. If it completes, the controller will likely come back online a few minutes after the update is complete

Completing this "Blind Update OS" can often restore to normal operation a controller that has its Operating System corrupted not allowing the Web page to be accessed, as long as you know the ACCNet ID and IP address (a reset IP can be performed) this process may be attempted.

It is also possible to flash an offline controller if it has reverted to the default IP address (169.254.1.1) and ACCNet ID of 1 if the Workstation is set to be in the same subnet so it can ping the controller and these default settings are used for the controller configuration.

If after a full cold restart and at least 2 attempts to flash the controller fail, then the controller may need to be returned for Repair.

Some possible causes of this problem are listed in What can cause a controller to reset, cold start or lose data.

Labels (1)
Labels:
  • Andover Continuum
Tags (5)
  • Find more articles tagged with:
  • 6920
  • blind
  • bootloader
  • mode
  • PaulFrost22
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.