Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Error: "No Entries in Database"

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Error: "No Entries in Database"
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
3139 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Error: "No Entries in Database"

Picard Product_Support
‎2018-09-06 02:16 PM

Last Updated: Crewman ContentModerator ‎2025-10-10 02:56 AM

Issue

  • Unable to connect to a system that is using Server/Client Configuration. After promoting a stand alone PC to a remote client and clicking on the connect button, an error "No Entries in Database" comes up and the user cannot connect to any of the controllers on the system.
  • After a restart of PC and an attempt to connect to the I/NET System, an error "No entries in database" is seen.

Product Line

TAC INET

Environment

  • I/NET Seven
  • Windows 7, Windows XP, Windows Vista, Windows 10

Cause

Some of the possible causes :

After promoting a stand alone PC to a remote client the Reference Host information of both the server and the client must be updated with the IP addresses of each other.

Bad communication or bad controller that is connecting the C-LAN to the Xenta 527

In some instances when running the I/NET IO Server as a service and after a restart of the PC hardware running a Windows 10 Operating System, it is has been seen to produce this "No entries in database" error.  At this stage the reason is currently unknown but the connection to the Xenta 527 is not made and the IO Server service needs to be restarted.

Resolution

  1. Open I/O Server
  2. Hit the Modify button
  3. In the Reference Host Column, add the IP address of the server
  4. Repeat steps 1-3 on the server, adding the IP address of the remote client.

Note: Should the Xenta 527 still not communicate to the controller:

  1. Verify that the C-LAN wire is connected properly
  2. There is communications between the controllers and the Xenta 527
  3. If not, unplug the C-Lan connector, from all the controllers and bring them online one at a time to determine which one could be bad.
  4. Replace possible bad controller and the system should come online again.

To correct the issue after a PC hardware restart, two options are available

  1. Restart the I/O Server service
  2. Change the run mode of the I/O Server to an application.  See Running I/NET Seven as a service on Windows for further information on options on how to achieve this. 
Labels (1)
Labels:
  • TAC INET
Tags (5)
  • Find more articles tagged with:
  • 4351
  • QC 85
  • Remote Client
  • RobertAndriolo19
  • server
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.