Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Ensuring the SSL Host Certificate and key file are a matching pair

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Ensuring the SSL Host Certificate and key file are a matching pair
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • David_Purser
    David_Purser
  • JonGreen
    JonGreen

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
3 Likes
4102 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Ensuring the SSL Host Certificate and key file are a matching pair

Picard David_Purser Picard
‎2022-12-02 09:46 AM

Issue

After configuring SSL certificates manually, having an incompatible Host Certificate and Key file can cause the import to EBO to fail.

Product Line

EcoStruxure Building Operation

Environment

  • Building Operation Enterprise Central
  • Building Operation Enterprise Server
  • Building Operation Automation Server

Cause

Host Certificate provides the public key for which the private key is paired. An unmatched Host Certificate and private key will cause the certificate import to fail.

Resolution

While managing certificates manually, it is recommended to check that the Host Certificate and Key files are a matching pair.

 

  1. Using the provided Host Certificate (.pem) file and private key (.key or .prv) file
  2. Download OpenSSL v1.1.1 Light choosing the EXE file type and correct version (Win64 or Win32), as the latest version letter will be posted to Win32/Win64 OpenSSL Installer for Windows - Shining Light Productions (slproweb.com) or OpenSSL installed with EBO
    1. If using Shining Light installer, it is recommended to open command prompt from where certificates are stored on the desktop and substitute openssl with "C:\Program Files\OpenSSL-Win64\bin\openssl.exe". Working with certificate files on the Windows desktop ensures the user will have the correct permission to run the commands, unlike putting certificate files in the Program Files directory where openssl.exe resides.
  3. Open PowerShell or Command Prompt
  4. Obtain the host certificate md5 hash with this command:
    1. openssl x509 -noout -modulus -in filename.pem | openssl md5
  5. Obtain the private key md5 hash using the command below. Use the correct command based on the key file file type
    1. openssl rsa -noout -modulus -in filename.prv | openssl md5
    2. openssl rsa -noout -modulus -in filename.key | openssl md5

 

In this example, the Host Certificate is HostCert.pem and the private key is EcoStruxure.key. The private key was converted to EcoStructure.prv using Step 12 of Installing an SSL Certificate from an External CA - Communities (se.com)

These commands make the hash more readable to human eye. We use openssl to inspect the x509 for Certificate and encryption type rsa for the key to produce the modulus (-modulus), which is a long string. You then use (-noout) to prevent the full modulus from printing to the screen. You then create a shorter md5 hash so the human eye can easily compare them. If the md5 hashes match, that indicates that the modulus is a match and proves that the certificate/key is a pair.

Commands.png

Labels (1)
Labels:
  • EcoStruxure Building Operation
Tags (2)
  • Find more articles tagged with:
  • DavidPurser22
  • DavidPurser23
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.