Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Deleting BACnet objects can permanently remove those objects from the BACnet device.

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Deleting BACnet objects can permanently remove those objects from the BACnet device.
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • GavinHe
    GavinHe
  • DavidFisher
    DavidFisher
  • AdamSteele
    AdamSteele
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
2414 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Deleting BACnet objects can permanently remove those objects from the BACnet device.

Picard Product_Support
‎2018-09-06 09:51 AM

Last Updated: Sisko GavinHe Sisko ‎2023-10-30 03:38 AM

Issue

Deleting BACnet objects using a BACnet Operator Workstation (BOWS) can permanently remove those objects from the BACnet device.  The effected devices can be Building Operation BACnet devices, e.g. Automation Server or third party BACnet devices.

Environment

  • Building Operation Enterprise Server
  • Building Operation Automation Server
  • 3rd Party BACnet Controllers

Cause

The BACnet controller(s) in question support BACnet create and delete services on the specific objects. 

Resolution

Functions as Designed

If the device supports create and delete services for the object it is designed to function this way.

GavinHe_1-1698659817027.png

In general the BOWS should provide as much as possible a complete and accurate image of the contents of the device.  For example using the Enterprise/Automation server as a BOWS: 

  • Creating new objects will automatically send a create-object request and attempt to create the object in the device.
  • Deleting objects will automatically send a delete-object request and attempt to delete the object in the device.
  • Upload and Download of object commands attempt to synchronize the database with the actual contents of the device. 
  • Download will attempt to create any objects that are in the database (but not in the device),
  • and also attempt to delete any objects from the device which are not in the database.
  • Upload adds or removes objects from the BOWS database.

Please see Protecting EBO/SBO BACnet objects from being deleted by 3rd party BOWS for a method of preventing BACnet points being deleted from an Enterprise/Automation Server.  Consult third party documentation to identify preventing creation/deletion.

 

Offline Workaround

If the device supports the Device Communication Control service, and allows disable, a work around is to make changes to the database while the device is offline.

GavinHe_2-1698660953599.png

For example, using the Enterprise/Automation server as a BOWS, right click the device and select Device->Communication->Disable.   

GavinHe_3-1698661317283.png

Open the property grid for the device and it should take about 12 seconds before the device is reported as offline.  Any other break in communication should also work to get the device offline.  Once offline, objects can be deleted from the database without affecting the device.  But, after changing the database this way, the device's "upload" or "download" commands should not be used, as it will re-synchronize the device and database (either deleting objects from the device, or adding them back to the database). 

It is important to note using this method the BOWS will not fully represent the objects in the device and also remember to re-enable the communication to the device.

Labels (1)
Labels:
  • EcoStruxure Building Operation
Tags (2)
  • Find more articles tagged with:
  • 15039
  • GavinHeward23
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.