Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Creating Windows Firewall rules to allow StruxureWare Building Operation to communicate on the TCP port

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Creating Windows Firewall rules to allow StruxureWare Building Operation to communicate on the TCP port
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
3 Likes
11853 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Creating Windows Firewall rules to allow StruxureWare Building Operation to communicate on the TCP port

Picard Product_Support
‎2018-09-10 10:40 PM

Last Updated: Crewman ContentModerator ‎2025-08-11 03:50 AM

Issue

Unable to establish communication between the enterprise and automation servers through the TCP Port 4444. Values are not being passed between the enterprise to the automation servers or between automation server to automation server.

Product Line

EcoStruxure Building Operation

Environment

  • Building Operation Enterprise Server
  • Building Operation Automation Server Premium
  • Building Operation Workstation

Cause

Windows Firewall is not allowing inbound or outbound information from passing through the TCP port 4444.

Resolution

First download and run TCP View. With TCP View running, sort the list by the Local Port and find all devices that are talking on port 4444. If the automation servers are in a state of LISTENING then rules must be created to allow communication. Copy the file path of SE.EnterpriseServer.exe in order to create the rules. This can be found by right clicking on one of the SE.EnterpriseServer.exe process > Process Properties... (C:\Program Files\Schneider Electric\StruxureWare 1.2\Enterprise Server\bin\SE.EnterpriseServer.exe)

If the automation servers are in the state of ESTABLISHED, then take a look at Binding between ES and AS or two AS shows Unresolved and "Communication Failed" Alarm occurs when Adding an AS. Source: /Server 1/Servers/ASL/System/Server C... for more troubleshooting help.


 

Change Windows Firewall Settings to Allow Programs

  1. Go to Start > Control Panel.
  2. Click on Windows Firewall.
  3. Click on "Allow a program or feature through Windows Firewall" on the left hand side of the window.
  4. Find "StruxureWare Building Operation" in the list of programs and make sure Home/Work and Public networks are selected. 

Note: If you do not have permission rights to make changes in this area of Windows, move on to the next section where you can set up inbound and outbound firewall rules.


 

Creating Inbound and Outbound Windows Firewall Rules

  1. Go to Start > Control Panel. 
  2. Click on Windows Firewall.
  3. Click "Advanced settings" on the left side of the window.
  4. Select Inbound Rules on the left side of the window and then click New Rule... on the right side of the window.
  5. On the first screen of the New Rule Wizard, choose Program. Click Next.
  6. In "This program path:" either browse to SE.EnterpriseServer.exe or paste the file path that was copied earlier from the TCP View into the box. Click Next.
  7. Select the option to "Allow the connection". Click Next.
  8. Leave Domain, Private, and Public checked unless otherwise desired. Click Next.
  9. Name the rule StruxureWare. Click Finish.
  10. Select Outbound Rules on the left side of the window and then click New Rule... on the right side of the window.
  11. Follow steps 5 through 9 to create the Outbound Rule.

Note that the SBO Firewall Config tool on the community can be used to automatically create the required firewall rules.

Labels (1)
Labels:
  • EcoStruxure Building Operation
Attachments
Tcpview.zip
Tags (2)
  • Find more articles tagged with:
  • 11354
  • RamaAly23
Was this article helpful? Yes No
75% helpful (3/4)
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.