Check the size of the SQL database for Vista trend logs and events

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Check the size of the SQL database for Vista trend logs and events
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • Cody_Failinger
    Cody_Failinger
  • CraigEl
    CraigEl
  • DavidFisher
    DavidFisher
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
1501 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Check the size of the SQL database for Vista trend logs and events

Picard Product_Support
‎2018-09-07 02:30 PM

Last Updated: Administrator CraigEl Administrator ‎2022-08-09 10:33 PM

Issue

Check the current size of the SQL database associated with a Vista database to ensure that it hasn't become full.

Product Line

TAC Vista

Environment

SQL

Cause

The SQL database that installs automatically with Vista has limitations on the amount of data it can hold.  Most often, this is plenty of space for many years of trending without issue.  But if a site is very old or has many trend logs defined, it can out grow the SQL database.  Limits are:

  • Vista IV - Vista 5.0.0 MSDE:  2 GB
  • Vista 5.0.1 - 5.1.6 SQL 2005 Express:  4 GB
  • Vista 5.1.7 and newer SQL 2008 Express:  10 GB

Resolution

This procedure checks the log size from the Vista Workstation:

  1. In Vista Workstation, click on the Vista Server in the folder pane
  2. Right click on $Backup_LDB and select Properties
  3. Scroll to the bottom and make note of the Database Size property (shown in grey).  This is the size of the database in MB.

This procedure checks the file size on the hard drive.  The assumption has been made that this is not a custom install, but the default SQL installed with Vista Server:

  1. Open Windows Explorer
  2. Navigate to C:\Program Files\Microsoft SQL Server\MSSQL.1\MSSQL\Data
  3. Locate files:
    • taclogdata.mdf
    • taclogdata_log.ldf
    Note:  If there are multiple instances of SQL installed on the PC, there may be MSSQL.1, MSSQL.2, MSSQL.3, etc.  Find the SQL instance that contains the file names listed above.
  4. Highlight both files and look at the bottom of the window on the status bar.  The combined size of these two files is shown.  This can be used to determine is the SQL database is full and requires a purge. 

To purge a Vista IV SQL database, see How to create a new database or purge a full SQL (i.e. it has hit the limit of 2G) in Vista IV.
To purge a Vista 5 SQL database, see Vista 5 full SQL database issue.

If purging is not an option, then the SQL will need to be upgraded to a full version of SQL (not express).  To see the different options, see Vista Database Sizing and SQL Server Selection.

Labels (1)
Labels:
  • TAC Vista
Tags (1)
  • Find more articles tagged with:
  • 4933
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.