Issue
A Continuum database configured for version 1.81 is not compatible with newer versions of the Continuum software.
Product Line
Andover Continuum
Environment
Continuum all versions
Cause
Continuum software and its database are version-dependent. Attempting to use a newer version of the software (e.g.1.9) with a database configured for an older version (e.g.,1.81) will result in incompatibility.
Resolution
To ensure proper functionality, the Continuum software version must match the database version exactly. For example:
- A database configured for version 1.81 will only work with software version 1.81.
- Attempting to use version 1.9 with a 1.81 database will fail.
This applies to all versions of Continuum. Always verify that both the software and database versions are aligned before deployment or upgrade.
Additional Notes
- This version dependency is critical for maintaining system stability and avoiding data access issues.
- Consider backing up your database before performing any upgrades.
- For upgrade paths or migration assistance, consult Schneider Electric support or your local technical representative.