Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Access Expert Installing SEQ Logs

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Access Expert Installing SEQ Logs
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • Alan_Wood
    Alan_Wood

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
2911 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Access Expert Installing SEQ Logs

Alan_Wood Leader
‎2023-06-05 05:02 PM

Last Updated: CraigEl Champion ‎2024-09-12 11:35 PM

Issue

Access Expert SEQ Log Installation Information

Product Line

EcoStruxure Access Expert

Environment

Access Expert Hosted V3

Cause

The SEQ Log is a valuable troubleshooting tool to be installed separately from Access Expert

Resolution

Overview

Access Expert utilizes a system logging application called SEQ which is used for troubleshooting and diagnostic purposes. While this service is not technically required to run any of the Feenics services, it provides valuable information when troubleshooting.


Downloading SEQ

The latest version can be downloaded at https://getseq.net/Download


Installing SEQ

Once the MSI is launched the wizard will prompt for installation as shown in the following Figures.

SEQ Welcome.png

SEQ EULA.png

SEQ Dest Folder.png

SEQ Ready Install.png

SEQ Complete.png


SEQ service installation dialog

SEQ Service.png

Once the SEQ logs are installed, click 'Browse Seq' button to open the log in the default browser.


Bookmark or Favorite

It may be beneficial to set the SEQ logs as a bookmark for easy access.

The example below is from Chrome.

SEQ Bookmark-Favorite.png


SEQ Settings

Click on the 'Settings' option at the top of the page to access and change the defaults.

SEQ Browse SEQ.png

Initially after clicking on Settings, the API keys page opens. Add an API key if required.


API Keys

SEQ API Keys.png


Retention Policy

From the settings page, select 'Retention' from the left-hand side menu.

Once at the Retention page, click add and set the retention policy. The Access Expert/Feenics default is 21 days. This is adjustable to your needs, however, it is recommended to never go below 7 days.

SEQ Retention.png

Note: Seq will periodically delete events covered by the policy based on their timestamp. Disk space will be reclaimed by a background compaction process and may not be available immediately.

Default is ‘all events’

SEQ Retention 2.png

SEQ Retention 3.png


Example Seq Log

SEQ Example.png

Note: Left Click once to expand an event and click it again to shrink it


Tips and Troubleshooting

  1. Ensure SEQ is installed on the PC where the Access Expert client is installed or it cannot ingest the Access Expert events.
  2. If a reinstall of SEQ is needed, manually deleting C:\ProgramData\Seq and subfolders is required after uninstalling SEQ from Windows Control Panel> Programs and Features.

    The SEQ uninstall does not remove the folder, subfolders and files.
    If the folder and files are not removed, the installation will fail.

  3. Before reinstalling SEQ, Grant the User that is running the installation full permissions to C:\ProgramData\Seq and subfolders if they do not have them.

    SEQ folder Permissions.png

  4. Installing SEQ using Windows Power Shell can be useful since it gives some feedback if something isn't working. Running the MSI installer within Windows doesn't give any feedback.

     

    Command syntax: 
    seq service install --listen=http://localhost:5341/ -u "YourPCName\admin" -p "YourAccountPassword"

    Note: The username must be specified as DOMAIN\user or MACHINE\user

    PowerShell Install Example:

    SEQ from Power Shell MSI.png
    SEQ from Power Shell.png

  5. SEQ Log documentation:

    1. https://docs.datalust.co/docs/getting-started

    2. https://docs.datalust.co/docs/ingestion-troubleshooting

Labels (1)
Labels:
  • EcoStruxure Access Expert
Tags (5)
  • Find more articles tagged with:
  • Access Expert
  • AlanWood23
  • AlanWood24
  • diagnostics
  • logs
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.