Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

64-bit operating systems with the Andover Continuum product line

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • 64-bit operating systems with the Andover Continuum product line
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
2713 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

64-bit operating systems with the Andover Continuum product line

Picard Product_Support
‎2020-09-16 07:14 PM

Last Updated: Crewman ContentModerator ‎2025-09-19 03:03 AM

Issue

Are 64-bit operating systems supported on the Andover Continuum product line?

Product Line

Andover Continuum

Environment

  • CyberStation
  • webClient

Cause

Compatibility requirements for Andover Continuum with 64-bit operating systems

Resolution

Release 1.93 and earlier:

  1. For all machines with CyberStation or webClient software installed, only operating systems running in 32-bit environments are supported. 64-bit environments are not supported. 
  2. However, for the Database Server on a LAN system where no Cyberstation or webClient software is installed, a 64-bit version of Windows Server 2008 (SP2) or Windows Server 2008 R2 may be used on systems running V1.92 and above. These will also require Microsoft SQL 2008 running in 64-bit mode.

Release 1.94 and later:

Release 1.94 supports 64-bit Operating Systems, however, Microsoft recommends the 32-bit version of Office 2010 because it prevents potential compatibility issues with other 32-bit applications, specifically third-party add-ins that are available only for 32-bit operating systems.

Please refer to the release notes for compatibility notes in specific versions.

Labels (1)
Labels:
  • Andover Continuum
Tags (2)
  • Find more articles tagged with:
  • 4514
  • CraigEllis20
Was this article helpful? Yes No
100% helpful (1/1)
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.