Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84527members
353770posts

Unplugging UPS at night

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

Solved
sml111_apc
Cadet
0 Likes
1
151

Unplugging UPS at night

This was originally posted on APC forums on 2/22/2009


When I am done using my PC at night and shut down the computer, the UPS stays on. Is this ok or should I unplug it from the wall when not in use? I just don't want it to overheat. The one used at work stays on 24/7 with no issues, which is why I am asking this. Thanks.


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
151

Re: Unplugging UPS at night

This reply was originally posted by Angela on APC forums on 2/23/2009


it is recommended that you leave the UPS on even when you shut your computer off. it is designed to be running all the time and turning it on and off frequently will probably shorten the overall life of the battery since the UPSs generally do a battery self test when being turned on and off. over time, if you did that each day, the battery would be used more often and thus need to be replaced sooner.

See Answer In Context

1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
152

Re: Unplugging UPS at night

This reply was originally posted by Angela on APC forums on 2/23/2009


it is recommended that you leave the UPS on even when you shut your computer off. it is designed to be running all the time and turning it on and off frequently will probably shorten the overall life of the battery since the UPSs generally do a battery self test when being turned on and off. over time, if you did that each day, the battery would be used more often and thus need to be replaced sooner.