Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

UPS Shutdown Settings Greyed Out on Back-UPS ES 750 using OS X 10.5.8

APC UPS for Home and Office Forum

Support forum to share knowledge about installation and configuration of APC offers including Home Office UPS, Surge Protectors, UTS, software and services.
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
  • APC UPS, Critical Power, Cooling and Racks
  • APC UPS for Home and Office Forum
  • UPS Shutdown Settings Greyed Out on Back-UPS ES 750 using OS X 10.5.8
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
BillP
Administrator BillP Administrator
2150
Teken
Kirk Teken
125
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
Solved Go to Solution
Back to APC UPS for Home and Office Forum
Start a Topic
Solved
Anonymous user
Not applicable

Posted: ‎2021-06-29 01:38 AM . Last Modified: ‎2024-03-22 03:13 AM

0 Likes
2
1176
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
Posted: ‎2021-06-29 01:38 AM . Last Modified: ‎2024-03-22 03:13 AM

UPS Shutdown Settings Greyed Out on Back-UPS ES 750 using OS X 10.5.8

I just received a Back-UPS ES 750 (Model # BE750G, S/N 3B0848X35129) yesterday and hooked it up to my MacBook, which is running OS X 10.5.8. I did at first install/uninstall the PowerChute software that came with the UPS. I then tried to configure using the operating system's Energy Saver. When I select UPS from Energy Saver, the energy settings "Sleep" and "Options" are active to accommodate changes. When I select the energy setting "UPS", I then see below the UPS battery level (100%) and the UPS model "Back-UPS ES 750 FW:841.I3 .D USB FW:I3". Below that, the shutdown choices: "Shutdown the computer when it has been on UPS power for:" AND "Shutdown the computer when the time left on UPS power is:" AND "Shutdown the computer when the UPS power level drops to:" are all greyed out, which prevents any changes. And yes, the "Click the lock to prevent further changes" is UNLOCKED. I have been searching through various threads on this issue and have not found a response for resolution. Right now, what I have is a UPS which will only delay the inevitable of loss of power with no graceful shutdown. BTW, I introduced a PowerBook, also running OS X 10.5.8, and get the same condition with that as well.

Message was edited by: jaycee2u

Labels
  • Labels:
  • Back-UPS & Surge Protectors
  • Tags:
  • be750g
  • energy_saver
  • macbook
  • os_x
  • powerbook
  • system_preferences
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
BillP
Administrator BillP Administrator
Administrator

Posted: ‎2021-06-29 01:38 AM . Last Modified: ‎2024-03-22 03:13 AM

0 Likes
0
1176
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
Posted: ‎2021-06-29 01:38 AM . Last Modified: ‎2024-03-22 03:13 AM

Hi John,

Unfortunately PCPE is not supported on 10.5.8 so having installed it there can be no guarantee what might have happened, though I doubt it caused this. Do you have the data cable direct to the computer or through a USB HUB? Are there any adapters or cable extenders being used? You can not click the check boxes either, correct? You might want to try to lock the options then unlock them again and see if it clears up.

See Answer In Context

Reply

Link copied. Please paste this link to share this article on your social media post.

Replies 2
Anonymous user
Not applicable

Posted: ‎2021-06-29 01:38 AM . Last Modified: ‎2024-03-22 03:13 AM

0 Likes
0
1176
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
Posted: ‎2021-06-29 01:38 AM . Last Modified: ‎2024-03-22 03:13 AM

Thank you for your reply. I had also connected UPS to my PowerBook, also running OS X 10.5.8, without installing the Powerchute SW. It too has the shutdown options grayed out where I can not check the boxes. I had toggled the lock/unlock feature as well. And yes, I have had the UPS cable connected directly to computer without any adapters, etc. I have since tried using Equinux's APC TRACKER and that product works great. The only problem is price ($129.00). Another solution that I have tried and is free is APCUPSD. I currently have it installed/configured and tested. I am working on CGI programs to allow for GUI status displays. I suppose with no support for OS X 10.5.8, this thread is pretty much dead. Again, thank you for your reply, I certainly appreciate it.

Reply

Link copied. Please paste this link to share this article on your social media post.

BillP
Administrator BillP Administrator
Administrator

Posted: ‎2021-06-29 01:38 AM . Last Modified: ‎2024-03-22 03:13 AM

0 Likes
0
1177
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
Posted: ‎2021-06-29 01:38 AM . Last Modified: ‎2024-03-22 03:13 AM

Hi John,

Unfortunately PCPE is not supported on 10.5.8 so having installed it there can be no guarantee what might have happened, though I doubt it caused this. Do you have the data cable direct to the computer or through a USB HUB? Are there any adapters or cable extenders being used? You can not click the check boxes either, correct? You might want to try to lock the options then unlock them again and see if it clears up.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.