Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84542members
353795posts

The APC Power Saving Back-UPS 750 is going to be good for my PSU ?

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

Solved
Chapapa07_apc
Crewman
Crewman
0 Likes
1
48

The APC Power Saving Back-UPS 750 is going to be good for my PSU ?

This was originally posted on APC forums on 6/20/2012


Someone told me in another forum that the psu OCZ Fatal1ty 550w (which is my actual PSU) needs a pure sine wave UPS, but I'm not sure, what do you think?.

My pc:
Core 2 quad q83002.5 ghz
MSI gtx 550 ti OC edition
4 gb ram ddr2 800
ecs g31tm7
PSU: OCZ Fatal1ty 550 w

I need a new usp because power outages are very common in my country, 99.9 % of them are not provoked by storms, so there are no spikes or surges when the electricity comes back.

My problem is that every time there is a power outage , my pc restarts itself when Im playing BF3 or crisis 2 (very heavy games) , my pc is plugged to a 300w ups but it seems like my ups is not enough for my PC consumption . When there is a power outage and I'm just surfing on the internet or watching movies my PC doesn't restart.

So, Im thinking about getting this UPS but Im not sure if the APC Power Saving Back-UPS 750 is gonna work for my PSU, I just want this UPS for turning off my pc properly when a power outage occurs , and not for keep playing until the electricity comes back.

Thank you in advance !

Message was edited by: Chapapa07


Accepted Solutions
Chapapa07_apc
Crewman
Crewman
0 Likes
0
48

Re: The APC Power Saving Back-UPS 750 is going to be good for my PSU ?

This was originally posted on APC forums on 6/22/2012


I just bought the apc Power Saving Back-UPS 750 , and its working fine wuth my usp when a power outage occurs, so the question was solved.

See Answer In Context

1 Reply 1
Chapapa07_apc
Crewman
Crewman
0 Likes
0
49

Re: The APC Power Saving Back-UPS 750 is going to be good for my PSU ?

This was originally posted on APC forums on 6/22/2012


I just bought the apc Power Saving Back-UPS 750 , and its working fine wuth my usp when a power outage occurs, so the question was solved.